Hi,
My requirement is Input 390Vdc +/-15V and Output 25V +/- 4V variation with 20Amp. Current. Is this design requirement is possible with LLC ? . Please share details if possible.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
My requirement is Input 390Vdc +/-15V and Output 25V +/- 4V variation with 20Amp. Current. Is this design requirement is possible with LLC ? . Please share details if possible.
Yes, LLC can be used for variable output applications. But in order to cover wide output range, we will need to have a lower magnetizing inductor inductance to series resonant inductor inductance ratio with a penalty of higher RMS current and lower efficiency than an LLC design with fixed output voltage.