Tool/software:
Hello TI,
Iam Designing a a buck converter using LM5116
Help me out in designing UVLO
How to calculate Ruv1 and Ruv2 and what should be the expected voltage and current at UVLO pin
Design values
- Input Voltage-Vin=50V~60V
- Output Voltage-Vout=5.2V
- Output Current=10A
- Output Ripple voltage=100mV expected
- Efficiency-ɳ=95% expected
- Switching Frequency=250kHz fixed w.r.t to the application circuit in datasheet.
I have used this formula for calculation. but couldn't solve it.
Thanking you,
K Bindhu.