This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: WEBENCH® Design Tools
Exporting the (screenie attached) webbench design fails, only when tina is selected as target. All the others work. Can webbench tina export be made to work? Thanks!
Oh, I made a screenie but see no attach button. I set webbench to 5-15V in, 12V 2A out. Chose 25118 design. Message is "export failed".
Hi DJ Nyberg,
Thank you for reporting this issue. We are working on a fix. We will let you know once it is resolved.
Thanks & Regards,
Praveen
Hi DJ Nyberg,
Seems simulations are disabled for LM25118 and simulation exports are enabled, hence the issue. I have disabled the simulation exports as well for this device. These changes should reflect on ti.com by the end of January 2020.
I went ahead and checked, simulation for family device (LM5118) which is enabled and only differs in Vin range with LM25118 (below E2E post for reference).
Reference post: https://e2e.ti.com/support/power-management/f/196/t/266981
You can use TINA exports from LM5118 for your input condition. I went ahead and exported the TINA files (attached below). Hope this helps.
/cfs-file/__key/communityserver-discussions-components-files/234/WBDesign7715_5F00_TINA_2D00_TI.zip
Best Regards,
Bhushan