Other Parts Discussed in Thread: LM5046, UCC2897A, LM5022
Hi team
Customer are evaluating PMP20551, and they need to change the output to 24VDC, which will lead to the change of transformer, loop comp, feedback network. By the way, they want to increase the frequency to minimize the total size. So I'm wondering if you have any insights for this requirement. I think the key is the transformer selection, so do we have a recommendation(ratio, Lp, or even specific device) for this requirement? Expect for your reply!