This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PMP20551: Changing the output voltage to 24VDC

Part Number: PMP20551
Other Parts Discussed in Thread: LM5046, UCC2897A, LM5022

Hi team

Customer are evaluating PMP20551, and they need to change the output to 24VDC, which will lead to the change of transformer, loop comp, feedback network. By the way, they want to increase the frequency to minimize the total size. So I'm wondering if you have any insights for this requirement. I think the key is the transformer selection, so do we have a recommendation(ratio, Lp, or even specific device) for this requirement? Expect for your reply!