This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
I am trying to simulate LME49721 in PSpice-for-TI .
First the simulation succeeded.
However I deleted capacitor2(C2), the simulation did not converge.
Output window:----------------------------------------------------------------------------------------------------------------------------------------
-------------- INFO(ORPROBE-3209): Simulation Profile: SCHEMATIC1-1 ---------------
INFO(ORPROBE-3183): Simulation running...
** Profile: "SCHEMATIC1-1" [ c:\Cadence\LME49721\SCHEMATIC1\1.sim]
Reading and checking circuit
Circuit read in and checked, no errors
Calculating bias point for Transient Analysis
Starting GMIN stepping
Starting power supply stepping
Starting pseudo-transient algorithm
INFO(ORPSIM-16594): To improve Pseudotransient Convergence and Performance, set following options to relax stabilization criteria for capacitor currents and inductor voltages: PTRANABSTOL=1e-5, PTRANVNTOL=1e-4
WARNING(ORPSIM-16354):Using high values of ITL4 for Speed Level > 0 may increase total simulation job time.
---------------------------------------------------------------------------------------------------------------------------------------------------------------
Why is this error occurring after only deleting capacitor?
Can someone answer this question?
Best Regards,
Mahoko
Hi Mahoko,
I'll take a look at this case and will get back to you with further comments in a couple days.
Best regards,
-Ivan Salazar
Applications Engineer - Low Power Audio & Actuators
Hello,
thank you for the response.
Actually I resolved this issue ,when I changed Maximum step size of Simulation Settings.
Thank you for your kindness.
Best Regards,
Mahoko