Tool/software:
Hi,
I am using CC2340R5_Q1 chip for our Digital key Project. Here i noticed that BLE example code form simplelink_lowpower_f3_sdk_8_40_00_61 SDK has 90% of RAM is used.
I have the requirement to complete the project within 70% of RAM memory.
Most of the memory consumed for RTOS, Can i able to make it on ROM as like CC2674 or CC1354
Hello,
I apologize for the delay in response. I will not be able to provide a response until early next week. Please expect a response on Tuesday 01/14.
Thanks,
Isaac
Hello Anto,
I do not believe this feature is available for CC2340R5-Q1 device. To optimize RAM consumption in software, please refer to RAM Optimization in the documentation.
Additionally, the CC2340R53-Q1 device is the same, but with almost double the RAM. You can view this device here.
Let me know if you have any additional questions.
Thanks,
Isaac