Hello,
Due to tirtos not being supported on Linux, I have been trying to get contiki to work on my cc2640f128 on my custom board. Specifically, the cc26x0-demo example from their platform-specific code: https://github.com/contiki-ng/contiki-ng/blob/develop/examples/platform-specific/cc26x0-cc13x0/cc26x0-demo.c.
Now I have been running into a few problems but most importantly the fact that i can see my chip boot-up and yet not advertise, the changes i made where as follows:
- Used the srf06 platform with the cc2640 board as a base and started removing any button/led hal related code on there since i am using my custom board (which to start is only powering my chip, no buttons or leds are being used)
- Altered the board.h file since the contiki one defines it for a 7x7mm packageand therefore used https://github.com/contiki-os/contiki/issues/2114 this post to guide me on the changes i need to make.
- Turned off the rom bootloader just as has been done on tirtos in order to eliminate any problems going wrong over there.
the platform.c file i used is shown below:
/* * Copyright (c) 2014, Texas Instruments Incorporated - http://www.ti.com/ * All rights reserved. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * 1. Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * 2. Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the distribution. * 3. Neither the name of the copyright holder nor the names of its * contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS * ``AS IS'' AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS * FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE * COPYRIGHT HOLDER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, * INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES * (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR * SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) * HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, * STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) * ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED * OF THE POSSIBILITY OF SUCH DAMAGE. */ /*---------------------------------------------------------------------------*/ /** * \addtogroup cc26xx-platforms * @{ * * \defgroup cc26xx-srf-tag SmartRF+CC13xx/CC26xx EM, SensorTags and LaunchPads * * This platform supports a number of different boards: * - A standard TI SmartRF06EB with a CC26xx EM mounted on it * - A standard TI SmartRF06EB with a CC1310 EM mounted on it * - The TI CC2650 SensorTag * - The TI CC1350 SensorTag * - The TI CC2650 LaunchPad * - The TI CC1310 LaunchPad * - The TI CC1350 LaunchPad * @{ */ #include "ti-lib.h" #include "contiki.h" #include "contiki-net.h" #include "lpm.h" #include "dev/leds.h" #include "dev/gpio-hal.h" #include "dev/oscillators.h" #include "ieee-addr.h" #include "ble-addr.h" #include "vims.h" #include "dev/cc26xx-uart.h" #include "dev/soc-rtc.h" #include "dev/serial-line.h" #include "rf-core/rf-core.h" #include "sys_ctrl.h" #include "uart.h" #include "sys/clock.h" #include "sys/rtimer.h" #include "sys/node-id.h" #include "sys/platform.h" #include "lib/random.h" #include "lib/sensors.h" #include "button-sensor.h" #include "dev/serial-line.h" #include "dev/button-hal.h" #include "net/mac/framer/frame802154.h" #include "board-peripherals.h" #include "driverlib/driverlib_release.h" #include <stdio.h> /*---------------------------------------------------------------------------*/ /* Log configuration */ #include "sys/log.h" #define LOG_MODULE "CC26xx/CC13xx" #define LOG_LEVEL LOG_LEVEL_MAIN /*---------------------------------------------------------------------------*/ /** \brief Board specific iniatialisation */ void board_init(void); /*---------------------------------------------------------------------------*/ #ifdef BOARD_CONF_HAS_SENSORS #define BOARD_HAS_SENSORS BOARD_CONF_HAS_SENSORS #else #define BOARD_HAS_SENSORS 1 #endif /*---------------------------------------------------------------------------*/ // static void // fade(leds_mask_t l) // { //*** you fade // volatile int i; // int k, j; // for (k = 0; k < 800; ++k) // { // j = k > 400 ? 800 - k : k; // leds_on(l); // for (i = 0; i < j; ++i) // { // __asm("nop"); // } // leds_off(l); // for (i = 0; i < 400 - j; ++i) // { // __asm("nop"); // } // } // } /*---------------------------------------------------------------------------*/ static void set_rf_params(void) { uint8_t ext_addr[8]; #if MAC_CONF_WITH_BLE ble_eui64_addr_cpy_to((uint8_t *)&ext_addr); NETSTACK_RADIO.set_object(RADIO_PARAM_64BIT_ADDR, ext_addr, 8); #else uint16_t short_addr; ieee_addr_cpy_to(ext_addr, 8); short_addr = ext_addr[7]; short_addr |= ext_addr[6] << 8; NETSTACK_RADIO.set_value(RADIO_PARAM_PAN_ID, IEEE802154_PANID); NETSTACK_RADIO.set_value(RADIO_PARAM_16BIT_ADDR, short_addr); NETSTACK_RADIO.set_value(RADIO_PARAM_CHANNEL, IEEE802154_DEFAULT_CHANNEL); NETSTACK_RADIO.set_object(RADIO_PARAM_64BIT_ADDR, ext_addr, 8); #endif } /*---------------------------------------------------------------------------*/ void platform_init_stage_one() { /* Enable flash cache and prefetch. */ ti_lib_vims_mode_set(VIMS_BASE, VIMS_MODE_ENABLED); ti_lib_vims_configure(VIMS_BASE, true, true); ti_lib_int_master_disable(); /* Set the LF XOSC as the LF system clock source */ oscillators_select_lf_xosc(); lpm_init(); board_init(); gpio_hal_init(); // leds_init(); // fade(LEDS_RED); /* * Disable I/O pad sleep mode and open I/O latches in the AON IOC interface * This is only relevant when returning from shutdown (which is what froze * latches in the first place. Before doing these things though, we should * allow software to first regain control of pins */ ti_lib_aon_ioc_freeze_disable(); HWREG(AON_SYSCTL_BASE + AON_SYSCTL_O_SLEEPCTL) = 1; ti_lib_sys_ctrl_aon_sync(); ti_lib_int_enable(INT_AON_GPIO_EDGE); ti_lib_int_master_enable(); soc_rtc_init(); // fade(LEDS_YELLOW); } /*---------------------------------------------------------------------------*/ void platform_init_stage_two() { random_init(0x1234); /* Character I/O Initialisation */ #if CC26XX_UART_CONF_ENABLE cc26xx_uart_init(); #endif serial_line_init(); #if BUILD_WITH_SHELL cc26xx_uart_set_input(serial_line_input_byte); #endif /* Populate linkaddr_node_addr */ #if MAC_CONF_WITH_BLE uint8_t ext_addr[8]; ble_eui64_addr_cpy_to((uint8_t *)&ext_addr); memcpy(&linkaddr_node_addr, &ext_addr[8 - LINKADDR_SIZE], LINKADDR_SIZE); #else ieee_addr_cpy_to(linkaddr_node_addr.u8, LINKADDR_SIZE); #endif // button_hal_init(); //fade(LEDS_GREEN); } /*---------------------------------------------------------------------------*/ void platform_init_stage_three() { radio_value_t chan = 0; radio_value_t pan = 0; set_rf_params(); NETSTACK_RADIO.get_value(RADIO_PARAM_CHANNEL, &chan); LOG_DBG("With DriverLib v%u.%u\n", DRIVERLIB_RELEASE_GROUP, DRIVERLIB_RELEASE_BUILD); // LOG_INFO(BOARD_STRING "\n"); LOG_DBG("IEEE 802.15.4: %s, Sub-GHz: %s, BLE: %s, Prop: %s\n", ti_lib_chipinfo_supports_ieee_802_15_4() == true ? "Yes" : "No", ti_lib_chipinfo_chip_family_is_cc13xx() == true ? "Yes" : "No", ti_lib_chipinfo_supports_ble() == true ? "Yes" : "No", ti_lib_chipinfo_supports_proprietary() == true ? "Yes" : "No"); // LOG_INFO(" RF: Channel %d", chan); if (NETSTACK_RADIO.get_value(RADIO_PARAM_PAN_ID, &pan) == RADIO_RESULT_OK) { // LOG_INFO_(", PANID 0x%04X", pan); } // LOG_INFO_("\n"); // #if BOARD_HAS_SENSORS // process_start(&sensors_process, NULL); // #endif //fade(LEDS_ORANGE); } /*---------------------------------------------------------------------------*/ void platform_idle() { /* Drop to some low power mode */ lpm_drop(); } /*---------------------------------------------------------------------------*/ /** * @} * @} */
The application example code that i am using is shown below:
/* * Copyright (c) 2014, Texas Instruments Incorporated - http://www.ti.com/ * All rights reserved. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * 1. Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * 2. Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the distribution. * 3. Neither the name of the copyright holder nor the names of its * contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS * ``AS IS'' AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS * FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE * COPYRIGHT HOLDER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, * INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES * (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR * SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) * HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, * STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) * ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED * OF THE POSSIBILITY OF SUCH DAMAGE. */ /*---------------------------------------------------------------------------*/ /** * \addtogroup cc26xx-platforms * @{ * * \defgroup cc26xx-examples CC26xx Example Projects * * Example projects for CC26xx-based platforms. * @{ * * \defgroup cc26xx-demo CC26xx Demo Project * * Example project demonstrating the CC13xx/CC26xx platforms * * This example will work for the following boards: * - cc26x0-cc13x0: SmartRF06EB + CC13xx/CC26xx EM * - CC2650 and CC1350 SensorTag * - CC1310, CC1350, CC2650 LaunchPads * * This is an IPv6/RPL-enabled example. Thus, if you have a border router in * your installation (same RDC layer, same PAN ID and RF channel), you should * be able to ping6 this demo node. * * This example also demonstrates CC26xx BLE operation. The process starts * the BLE beacon daemon (implemented in the RF driver). The daemon will * send out a BLE beacon periodically. Use any BLE-enabled application (e.g. * LightBlue on OS X or the TI BLE Multitool smartphone app) and after a few * seconds the cc26xx device will be discovered. * * - etimer/clock : Every CC26XX_DEMO_LOOP_INTERVAL clock ticks the LED defined * as CC26XX_DEMO_LEDS_PERIODIC will toggle and the device * will print out readings from some supported sensors * - sensors : Some sensortag sensors are read asynchronously (see sensor * documentation). For those, this example will print out * readings in a staggered fashion at a random interval * - Buttons : CC26XX_DEMO_TRIGGER_1 button will toggle CC26XX_DEMO_LEDS_BUTTON * - CC26XX_DEMO_TRIGGER_2 turns on LEDS_REBOOT and causes a * watchdog reboot * - The remaining buttons will just print something * - The example also shows how to retrieve the duration of a * button press (in ticks). The driver will generate a * sensors_changed event upon button release * - Reed Relay : Will toggle the sensortag buzzer on/off * * @{ * * \file * Example demonstrating the cc26xx platforms */ #include "contiki.h" #include "sys/etimer.h" #include "sys/ctimer.h" #include "dev/leds.h" #include "dev/watchdog.h" #include "dev/button-hal.h" #include "random.h" #include "button-sensor.h" #include "batmon-sensor.h" #include "board-peripherals.h" #include "rf-core/rf-ble.h" #include "ti-lib.h" #include <stdio.h> #include <stdint.h> /*---------------------------------------------------------------------------*/ #define CC26XX_DEMO_LOOP_INTERVAL (CLOCK_SECOND * 20) #define CC26XX_DEMO_LEDS_PERIODIC LEDS_YELLOW #define CC26XX_DEMO_LEDS_BUTTON LEDS_RED #define CC26XX_DEMO_LEDS_REBOOT LEDS_ALL /*---------------------------------------------------------------------------*/ // #define CC26XX_DEMO_TRIGGER_1 BOARD_BUTTON_HAL_INDEX_KEY_LEFT // #define CC26XX_DEMO_TRIGGER_2 BOARD_BUTTON_HAL_INDEX_KEY_RIGHT // #if BOARD_SENSORTAG // #define CC26XX_DEMO_TRIGGER_3 BOARD_BUTTON_HAL_INDEX_REED_RELAY // #endif /*---------------------------------------------------------------------------*/ static struct etimer et; /*---------------------------------------------------------------------------*/ PROCESS(cc26xx_demo_process, "cc26xx demo process"); AUTOSTART_PROCESSES(&cc26xx_demo_process); /*---------------------------------------------------------------------------*/ #if BOARD_SENSORTAG /*---------------------------------------------------------------------------*/ /* * Update sensor readings in a staggered fashion every SENSOR_READING_PERIOD * ticks + a random interval between 0 and SENSOR_READING_RANDOM ticks */ #define SENSOR_READING_PERIOD (CLOCK_SECOND * 20) #define SENSOR_READING_RANDOM (CLOCK_SECOND << 4) // #define printf () static struct ctimer bmp_timer, opt_timer, hdc_timer, tmp_timer, mpu_timer; /*---------------------------------------------------------------------------*/ static void init_bmp_reading(void *not_used); static void init_opt_reading(void *not_used); static void init_hdc_reading(void *not_used); static void init_tmp_reading(void *not_used); static void init_mpu_reading(void *not_used); /*---------------------------------------------------------------------------*/ static void print_mpu_reading(int reading) { if (reading < 0) { printf("-"); reading = -reading; } printf("%d.%02d", reading / 100, reading % 100); } /*---------------------------------------------------------------------------*/ static void get_bmp_reading() { int value; clock_time_t next = SENSOR_READING_PERIOD + (random_rand() % SENSOR_READING_RANDOM); value = bmp_280_sensor.value(BMP_280_SENSOR_TYPE_PRESS); if (value != CC26XX_SENSOR_READING_ERROR) { printf("BAR: Pressure=%d.%02d hPa\n", value / 100, value % 100); } else { printf("BAR: Pressure Read Error\n"); } value = bmp_280_sensor.value(BMP_280_SENSOR_TYPE_TEMP); if (value != CC26XX_SENSOR_READING_ERROR) { printf("BAR: Temp=%d.%02d C\n", value / 100, value % 100); } else { printf("BAR: Temperature Read Error\n"); } SENSORS_DEACTIVATE(bmp_280_sensor); ctimer_set(&bmp_timer, next, init_bmp_reading, NULL); } /*---------------------------------------------------------------------------*/ static void get_tmp_reading() { int value; clock_time_t next = SENSOR_READING_PERIOD + (random_rand() % SENSOR_READING_RANDOM); value = tmp_007_sensor.value(TMP_007_SENSOR_TYPE_ALL); if (value == CC26XX_SENSOR_READING_ERROR) { printf("TMP: Ambient Read Error\n"); return; } value = tmp_007_sensor.value(TMP_007_SENSOR_TYPE_AMBIENT); printf("TMP: Ambient=%d.%03d C\n", value / 1000, value % 1000); value = tmp_007_sensor.value(TMP_007_SENSOR_TYPE_OBJECT); printf("TMP: Object=%d.%03d C\n", value / 1000, value % 1000); SENSORS_DEACTIVATE(tmp_007_sensor); ctimer_set(&tmp_timer, next, init_tmp_reading, NULL); } /*---------------------------------------------------------------------------*/ static void get_hdc_reading() { int value; clock_time_t next = SENSOR_READING_PERIOD + (random_rand() % SENSOR_READING_RANDOM); value = hdc_1000_sensor.value(HDC_1000_SENSOR_TYPE_TEMP); if (value != CC26XX_SENSOR_READING_ERROR) { printf("HDC: Temp=%d.%02d C\n", value / 100, value % 100); } else { printf("HDC: Temp Read Error\n"); } value = hdc_1000_sensor.value(HDC_1000_SENSOR_TYPE_HUMID); if (value != CC26XX_SENSOR_READING_ERROR) { printf("HDC: Humidity=%d.%02d %%RH\n", value / 100, value % 100); } else { printf("HDC: Humidity Read Error\n"); } ctimer_set(&hdc_timer, next, init_hdc_reading, NULL); } /*---------------------------------------------------------------------------*/ static void get_light_reading() { int value; clock_time_t next = SENSOR_READING_PERIOD + (random_rand() % SENSOR_READING_RANDOM); value = opt_3001_sensor.value(0); if (value != CC26XX_SENSOR_READING_ERROR) { printf("OPT: Light=%d.%02d lux\n", value / 100, value % 100); } else { printf("OPT: Light Read Error\n"); } /* The OPT will turn itself off, so we don't need to call its DEACTIVATE */ ctimer_set(&opt_timer, next, init_opt_reading, NULL); } /*---------------------------------------------------------------------------*/ static void get_mpu_reading() { int value; clock_time_t next = SENSOR_READING_PERIOD + (random_rand() % SENSOR_READING_RANDOM); printf("MPU Gyro: X="); value = mpu_9250_sensor.value(MPU_9250_SENSOR_TYPE_GYRO_X); print_mpu_reading(value); printf(" deg/sec\n"); printf("MPU Gyro: Y="); value = mpu_9250_sensor.value(MPU_9250_SENSOR_TYPE_GYRO_Y); print_mpu_reading(value); printf(" deg/sec\n"); printf("MPU Gyro: Z="); value = mpu_9250_sensor.value(MPU_9250_SENSOR_TYPE_GYRO_Z); print_mpu_reading(value); printf(" deg/sec\n"); printf("MPU Acc: X="); value = mpu_9250_sensor.value(MPU_9250_SENSOR_TYPE_ACC_X); print_mpu_reading(value); printf(" G\n"); printf("MPU Acc: Y="); value = mpu_9250_sensor.value(MPU_9250_SENSOR_TYPE_ACC_Y); print_mpu_reading(value); printf(" G\n"); printf("MPU Acc: Z="); value = mpu_9250_sensor.value(MPU_9250_SENSOR_TYPE_ACC_Z); print_mpu_reading(value); printf(" G\n"); SENSORS_DEACTIVATE(mpu_9250_sensor); ctimer_set(&mpu_timer, next, init_mpu_reading, NULL); } /*---------------------------------------------------------------------------*/ static void init_bmp_reading(void *not_used) { SENSORS_ACTIVATE(bmp_280_sensor); } /*---------------------------------------------------------------------------*/ static void init_opt_reading(void *not_used) { SENSORS_ACTIVATE(opt_3001_sensor); } /*---------------------------------------------------------------------------*/ static void init_hdc_reading(void *not_used) { SENSORS_ACTIVATE(hdc_1000_sensor); } /*---------------------------------------------------------------------------*/ static void init_tmp_reading(void *not_used) { SENSORS_ACTIVATE(tmp_007_sensor); } /*---------------------------------------------------------------------------*/ static void init_mpu_reading(void *not_used) { mpu_9250_sensor.configure(SENSORS_ACTIVE, MPU_9250_SENSOR_TYPE_ALL); } #endif /*---------------------------------------------------------------------------*/ // static void // get_sync_sensor_readings(void) // { // int value; // printf("-----------------------------------------\n"); // value = batmon_sensor.value(BATMON_SENSOR_TYPE_TEMP); // printf("Bat: Temp=%d C\n", value); // value = batmon_sensor.value(BATMON_SENSOR_TYPE_VOLT); // printf("Bat: Volt=%d mV\n", (value * 125) >> 5); // #if BOARD_SMARTRF06EB // SENSORS_ACTIVATE(als_sensor); // value = als_sensor.value(0); // printf("ALS: %d raw\n", value); // SENSORS_DEACTIVATE(als_sensor); // #endif // return; // } /*---------------------------------------------------------------------------*/ // static void // init_sensors(void) // { // SENSORS_ACTIVATE(batmon_sensor); // } /*---------------------------------------------------------------------------*/ // static void // init_sensor_readings(void) // { // #if BOARD_SENSORTAG // SENSORS_ACTIVATE(hdc_1000_sensor); // SENSORS_ACTIVATE(tmp_007_sensor); // SENSORS_ACTIVATE(opt_3001_sensor); // SENSORS_ACTIVATE(bmp_280_sensor); // init_mpu_reading(NULL); // #endif // } /*---------------------------------------------------------------------------*/ PROCESS_THREAD(cc26xx_demo_process, ev, data) { PROCESS_BEGIN(); // printf("CC26XX demo\n"); // init_sensors(); /* Init the BLE advertisement daemon */ rf_ble_beacond_config(0, BOARD_STRING); rf_ble_beacond_start(); etimer_set(&et, CC26XX_DEMO_LOOP_INTERVAL); //get_sync_sensor_readings(); //init_sensor_readings(); while (1) { PROCESS_YIELD(); if (ev == PROCESS_EVENT_TIMER) { if (data == &et) { // leds_toggle(CC26XX_DEMO_LEDS_PERIODIC); //get_sync_sensor_readings(); etimer_set(&et, CC26XX_DEMO_LOOP_INTERVAL); } } // else if (ev == button_hal_periodic_event) //{ // button_hal_button_t *button = data; // printf("%s periodic event, duration %d seconds\n", // BUTTON_HAL_GET_DESCRIPTION(button), // button->press_duration_seconds); //} //else if (ev == button_hal_release_event) //{ // button_hal_button_t *btn = (button_hal_button_t *)data; // printf("%s release event\n", BUTTON_HAL_GET_DESCRIPTION(btn)); // if (btn->unique_id == CC26XX_DEMO_TRIGGER_1) // { // // leds_toggle(CC26XX_DEMO_LEDS_BUTTON); // } // else if (btn->unique_id == CC26XX_DEMO_TRIGGER_2) // { // // leds_on(CC26XX_DEMO_LEDS_REBOOT); // // watchdog_reboot(); // #if BOARD_SENSORTAG // } // else if (btn->unique_id == CC26XX_DEMO_TRIGGER_3) // { // if (buzzer_state()) // { // buzzer_stop(); // } // else // { // buzzer_start(1000); // } // } // } // else if (ev == sensors_event) // { // if (data == &bmp_280_sensor) // { // get_bmp_reading(); // } // else if (data == &opt_3001_sensor) // { // get_light_reading(); // } // else if (data == &hdc_1000_sensor) // { // get_hdc_reading(); // } // else if (data == &tmp_007_sensor) // { // get_tmp_reading(); // } // else if (data == &mpu_9250_sensor) // { // get_mpu_reading(); // #endif // } //} } PROCESS_END(); } /*---------------------------------------------------------------------------*/ /** * @} * @} * @} */
I am not sure why my chip is not advertising, I have hooked it up and downloaded tirtos stack and simple periphiral app in windows and got it to work, yet I have not been successful on linux/contiki, can anyone offer any help/direction on what to try? I am running out of ideas!
Thanks guys!
Asma