Hello,
The datasheet for the TRF7970A states that it supports ISO 18000-3, however there I can find almost nothing regarding this standard in the documentation for TRF7970A.
We would like to be able to read/write the NXP ICode ILT-M tags, which use ISO 18000-3 Mode 3. We have had no success so far using the TRF7970 EVM Control GUI; we can succesfully read the UID on some 14443A tags, but the 18000-3 tags do not show up.
Is ISO 18000-3 Mode 3 not natively supported in the firmware?
Thanks in advance,
Anders