Part Number: CC1312R7
I am Francis daCosta, CTO meshdynamics.
Please see https://meshdynamics.com/Chirp_Primer.html and https://meshdynamics.com/CHIRP/Chirp_Primer_Slides.pdf for overview on this Soft Chips (tm)project.
The main customer is still the military. The intent is to provide deep end to end secure SMS messaging globally. A version was built and tested.
We now want to build a low cost low power version to be produced in millions for military and food systems, and climate preparedness and pollution monitoring etc. Patents awarded and pending. Code exists but needs a full rewrite to work on commercial US based chipsets as part of CHIPS initiative objectives.
Please see use cases here https://meshdynamics.com/Soft_Chips.html
i need details on implementation for my engineers. If TI engineers are not available please point me to where i can find qualified contractors or developers to help me.
The project is funded. We want to use FreeRTOS or Zephyr. Code must be Posix compliant and transportable to other ti devices. We will use CC1312R7, its launch pad and the SensorTags to prove the secure end to end connection from edge to cloud using enterprise customized carrier pigeons and enterprise customized edge devices with UART connections between the two and BLE to BLE paired file transfers between carrier pigeon and connected device e.g smartphone. Please see slides 8,9,10.
francis dacosta 4083737700 fdacosta@meshdynamics.com or fdacosta@gmail.com (preferred)