Other Parts Discussed in Thread: UNIFLASH, , CC1310, WMBUS, CC1350
Hi!
I'm trying to flash a launchxl-cc1312r1 with "Serial_CC13xx_Collector_T2.hex", so I can communicate with the device via the SATP API Interface. I have used Uniflash to flash my device with "Serial_CC13xx_Collector_T2.hex" found in "wmbus-cc13xx-rtos-2.0.0". Here I just added the .hex file.
When sending a ping (found this example in an older thread) nothing happens.
Sending "A5 00 03 FF FC 00 00 0A 53 78" 115200@8N1 on the USB port (Application/User UART).
Do I need to flash the device with more than just the .hex file mentioned?
/Gvl