This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-CC1310: LAUNCHXL-CC1310:

Part Number: LAUNCHXL-CC1310
Other Parts Discussed in Thread: CC1310

After building Project for pwmled2_CC1310_LAUNCHXL_tirtos_gcc I am getting the below mentioned window, The target become connected but DI06 and DI07 Led don't active. How will I solve this? I am a beginner  in CC1310, Than you.

  • Please state what SDK version you are using and your CCS.

    I imported the project from the latest SDK (4_20) and used CCS 9.1

    I did not experience any problems, downloading, debugging and running the code.

    Siri

  • I am using simplelink_cc13x0_sdk_4_20_02_07, and CCS V11.

  • Please use the version recommended in the release note for the SDK version you are using:

    Dependencies

    SimpleLinkTm CC13x0 SDK 4.20.02.07 was built & tested on a Windows 7 host platform using the following Integrated Development Environment (IDE) and components. Using an IDE version or TI-RTOS version not listed below may result in compatibility issues with this SDK release.

    I have tested it and it works, so not possible for me to know what is going on on your end since I am not able to reproduce the problem. 

    I would assume that the pwmled2_CC1310_LAUNCHXL_tirtos_gcc is not the only one that you are not able to run?

    Also, have you tested your LP with SmartRF Studio and confirmed that it works properly there?

    Siri

  •  pwmled2_CC1310_LAUNCHXL_tirtos_ccs is not working,  

    No, I have not tested LP with SmartRF Studio.

    Thank you very much for your response. 

  • Hi, Thanks for your guidance, the launchpads are working fine. 

    Will you please guide me, on how to upload the program in the customized CC1310F128RMS CKT board? Lots of thanks for your time.

  • Please see the following:

    https://www.ti.com/lit/swra640

    Siri

  • Hi Siri,

    Thanks for your guidelines, Will you please explain how these boards are connected for uploading the program to the customized board? 

  • I am not familiar with your custom board, so I cannot tell you how to connect it.

    Please see the following post that explains how the CC1310 LP can be used to debug an external target:

    (+) LAUNCHXL-CC1310: using xds110 jtag to debug external targets - Sub-1 GHz forum - Sub-1 GHz - TI E2E support forums

    Siri

  • Hi! Thank you for your cordial support. When I tried to upload the code, he closed contact with the customized turn on the LED light of the launchpad. What could be the reason?

  • I am sorry, but I do not think I can help you. I do not even understand what you are struggling with, as I do not know the HW you are connecting to the LP and what you are trying to do with it.

    SIri

  • Hi Siri, you helped me a lot. Can we have a 101 meeting through Zoom or Google Meet if you are comfortable? 

    Thank you. 

  •  Hi I am trying to upload code in the green PCB(CC1310 customized board) but it is showing error Error connecting to the target:
    (Error -242 @ 0x0)
    A router subpath could not be accessed.
    The board configuration file is probably incorrect.
    (Emulation package 9.6.0.00172)
    And when I am trying to use Smart RF flash programmer 2 it shows 

    >Initiate access to target: COM7 using 4-pin cJTAG.

    >No response from device. Device may not be in bootloader mode. Reset device and try again.

    If problem persists, check connection and baud rate.

    >Connecting over serial bootloader failed: No response from device. Device may not be in bootloader mode. Reset device and try again.

    If problem persists, check connection and baud rate.

    >Failed to create device object.

    Seeking help to solve this please. 

  • I am sorry but I cannot provide any other help than the following (as I have shared before)

    https://www.ti.com/lit/swra640

    Siri