This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI,
I have two cc1125 devices. I need to find out the maximum distance it can communicate. Right now, the easy link test works only for 500 meters. But in one of the youtube videos from TI and couple of forums I could see people getting more range liek 25km. Can anyone say what setting I should keep my device to achieve the maximum distance.
Viswanath,
From this E2E thread, RGW states the settings he used as well as the board that was used for his test.
Are you using your own custom board? Or the CC1125 development kit?
BR,
Seong
Have you calculated the estimated range with the RF parameters you are using with http://www.ti.com/tool/RF-RANGE-ESTIMATOR?
I repeat my question: Have you calculated the estimated range with the RF parameters you are using with http://www.ti.com/tool/RF-RANGE-ESTIMATOR?
The range is dependent on datarate etc so without knowing exactly what you are testing with it's not possible to know the expected range. Please note that you also have to take into account the noise floor when you use the excel sheet since if you have a high background noisefloor the range will be lower.
All i wanted is how much distance the devices can cover while they communicate. I wanted to replace the rf433 Mhz with these devices. Yes, I saw the excel sheet after you told me to. I do not know how to calculate the noise floor interference since I am new to RF. I tried all the settings in the demo kit and all I could get is less than 500 meters. Can you guide me on how to measure the background noise floor. I am a newbie here and any help would be of great use to me.
To measure the background noise: Connect one of your board and open SmartRF Studio (You want only one board in RX, no known TX sources). Open the cont RX tab and see which RSSI you get. This is your background noise.
Thank you. Do i have to program the boards through smart rf studio before taking them out in the field or i can adjust the settings directly in the demo board? Can you please suggest what values will you keep in the demo kit for "PER Test" to achieve maximum distance.
This is for a narrow RX BW. Could you repeat the test with the setting you use in the range test? Which datarte etc are you using?
I use data rate as 1.2kbps and frequency as 915Mhz. I do not know the RX filter BW and deviation frequency so I kept that to default values and I still get the same values.
In the demo kit on the LCD screen what I use is,
PER Test -> Expert Mode -> Manual mode -> 915Mhz -> Master -> one-way.
with data as 1.2kbps and TX Power as 14dBm.
In another demo kit, I click the same settings with slave mode. I used to walk around the master device to decide the range and it is limited to only 500 meters.
Viswanath,
Now that you have the required parameters, using the RF Range Estimator, what is the distance calculated? Please share a screenshot.
Thanks,
Seong
Can you suggest what Ideal parameters should I use in the demo kit. I am testing the devices in the soccer field nearby. So please give me out values from your side and I will try those values.
Your latest question is basically the same that you have asked in this thread: https://e2e.ti.com/support/wireless-connectivity/sub-1-ghz/f/156/t/860862
Have you tested using packet Rx/ Tx now?
Viswanath,
Since you have two threads covering the same topic, I will be closing this one so that this discussion can be continued on a single thread --> CC1125DK: Parameters for maximum distance in smart RF studio - Sub-1 GHz forum - Sub-1 GHz - TI E2E support...
BR,
Seong