Part Number: WL1837MOD
Dear Sir,
We have integrated WL1837MODGIMOCR in the design and currently the product is going for pre-compliance/certification testing.
As per comment from Test Lab, during certification testing for WiFi , it is required for the module to be in continuous transmit mode for more than 45 mins with (Carrier + data) and the power of the signal should be atleast 16dBm.
We are issuing the following the commands as given in WL Calibrator user guide,section 3.8
3.8 Example TX Output With Different Settings
The below section provides examples of using the commands for different modes of transmission and TX
channel occupancy. All TX examples are 50% DC and include "channel limits" to compensate the limitations
from INI file
Band 2.4 GHz, 11B
calibrator wlan0 wl18xx_plt stop_tx
calibrator wlan0 wl18xx_plt tune_channel 7 0 1
calibrator wlan0 wl18xx_plt set_tx_power 20000 0 0 7 0 0 0 1 0 0 0 0
calibrator wlan0 wl18xx_plt start_tx 500 3 500 0 0 1 0 0 00:11:22:33:44:55 01:02:03:04:05:06 0
However we have the following issues:
1) The module is only transmitting for 2-3 mins and then getting OFF
2)The observed signal power on the spectrum analyzer is about -40dBm
So pls. let us know
1) How to put in Continuous Transmit mode for longer duration > 45 mins , with power level of 16dBm.
2)How to vary the power to different levels(dB)
3)How to change between modes a/b/g/n
4)How to change above parameters similarly for Receive mode.
SK Mohanty