Other Parts Discussed in Thread: CC3235S, UNIFLASH, SYSCONFIG, , TMS570LC4357, MSP430FR5969
Hello Team,
I've been facing an issue programming (debugging/flashing) my LaunchXL-CC3235 device.
Application: Data Transmission through 802.11 over UDP protocol
Issue:
I was trying to program my LaunchXL-CC3235 device. Tool: CCS V11 and CC3235S SDK V6.10.
I imported built in program for UDP loopback, built the code and entered the debug mode. I then updated code and checked for the required parameters through Debug mode only. Once completed, I flashed the program using CCS only. Then on, I'm receiving below specified error.

I also tried work-arounds suggested in various posts. Link to them are as follows:
- https://www.youtube.com/watch?v=-yGmq_VKvTQ
- https://e2e.ti.com/support/microcontrollers/msp-low-power-microcontrollers-group/msp430/f/msp-low-power-microcontroller-forum/494211/issues-with-the-debug-xds110-and-msp432/1786284#1786284
- https://e2e.ti.com/support/microcontrollers/msp-low-power-microcontrollers-group/msp430/f/msp-low-power-microcontroller-forum/865406/ccs-msp432p401r-cs_dap_0-error-connecting-to-the-target-error--1170-0x0-unable-to-access-the-dap
However, no success.
While I check for the connection, it shows successful as shown below.

So, my query is, how do I fix the issue?
P.S. 1: My last flashed code is still working as my device is being shown as WiFi available network with the specified settings.
P.S. 2: Only one time I've flashed this devise.
Regards,
H C Trivedi