Other Parts Discussed in Thread: SYSCONFIG
Hi everyone
There is a locked thread with the exact same title... The answer from Shlomi helped there:
"Looks like the CCS version is OK and you are having some incompatibilities with sysconfig.
From the SDK I could see it was designed and tested with Sysconfig 1.15.
Can you install it and set it in CCS so 1.15 is used instead of 1.12?"
I happen to have that problem a lot in various examples.
Where can I see, which version of sysconfig the example was designed for?
If I need to change the Sysconfig version, do I really need to delete the not used version from the filesystem and copy the correct one into a folder where CCS can discover it? I hope, there's a better way...
Kind regards
Christian