Tool/software:
Dear TI Sirs:
The CC33XX-LINUX-MPU v1.0.0.5 release on 2024/07/31 has a strange situation after issuing the Standard LE_Transmitter_Test HCI command.
The radio signal observed from Spectrum Analyzer or the LitePoint IQxel test equipment will stop automatically after a period of time. And the btmon did not find any LE_Test_End event.
I ever post some similar situations before on below threads:
And I got 1 unofficial release firmware from TI to test after v1.0.0.3, that fix the problem and got the response saying will fixed in the next coming version of the firmware.
However, it is NOT fixed in v1.0.0.4 and the LE_Transmitter_Test will still end with a LE_Test_End HCI command around 38 seconds.
Then I find the v1.0.0.5 is released on 07/31/2024 and tested on this, at this version, by using btmon, after issuing LE_Transmitter_Test command, the LE_Test_End did not show up, but the radio signal is not emitting after a period of time.
We are using this HCI command during the production/verification, do you know when it will fix or do you have any other Vendor Specific HCI command that can emit the BLE radio signal continuously?
Regards,
/ckhsu