Other Parts Discussed in Thread: SIGCONARCHITECT Downloading of SigCon Architect from TI.com and install works successfully. However, when attempting to open the SigCon Architect GUI, the GUI loads with half the GUI off-screen to the right and an error…
Two common interfaces used to control brushed DC motors are Phase/Enable (PH/EN) and PWM. Both of these interfaces require 2 signals to be able to fully control brushed DC motors or other types of load connected to the outputs of a motor driver.
Phase…
Part Number: PROCESSOR-SDK-DRA8X-TDA4X
This article explains how to build sysfw.itb file for J7ES-HS device. It assumes that PSDKLA is installed and setup correctly as explained in the link: software-dl.ti.com/.../index.html
Part Number: TLV320AIC3254EVM-K
My customer is having issues getting the Eval Board started. It is connected via USB (D2 lights up). But when the GUI is launched nothing is displayed and here is an image of what we're getting:
I changed the settings…
Q: How can I learn about multicore development on C2000?
Take a look at the C2000 Multicore Development User's Guide ( https://software-dl.ti.com/C2000/docs/C2000_Multicore_Development_User_Guide/index.html )
Other Parts Discussed in Thread: DRV8313 , DRV8312 , DRV8332 , DRV10964 , DRV10970 , DRV10974 , DRV10975 , DRV10983 , DRV10983-Q1 , DRV10987 Understanding the parameters of a motor is very important in selecting a motor driver as the rating of the FETs…