Hi all,
I'm designing a schematic using AM3358ZCZD72 device.
I'm confusing about clock circuit design when compare the reference design and Advisory 1.0.30: OSC0 and OSC1: "Noise immunity improved when Crystal Circuit is connected directly to PCB…
Hi all,
I'm designing a schematic using AM3358ZCZD72 device.
I'm confusing about clock circuit design when compare the reference design and Advisory 1.0.30: OSC0 and OSC1: "Noise immunity improved when Crystal Circuit is connected directly to PCB…
I will try to reproduce this after the holidays since I dont have a BBB + proper development environment at hand. Until now I use this (still unsatisfying because not always working) workaround:
In pm33xx.c I activate the self refresh in PWR_MGMT_CTRL…
Hi Arthur,
For this fail (complain about gen_test_char), when cross compiling Apache, check the hacks described here: https://groups.google.com/forum/#!topic/dealextreme-nas-/lmW1PdGEWA0
Also this guide may be of some help: http://myurc.org/tools/UCHe…
Hi,
thanks for the reply and the hints.
My wakeup sources seem to be okay:
root@android:/sys/kernel/debug # cat wakeup_sources
name active_count event_count hit_count active_since total_time max_time last_change
gpio-keys 0 0 0 0 0 0 0
am33xx-rtc 0 0 0 0…
HI
I am using the am3358.Now the system startup time is 19 secconds.
U-Boot SPL 2011.09 (Oct 04 2014 - 18:17:24)
Texas Instruments Revision detection unimplemented
U-Boot 2011.09 (Oct 04 2014 - 18:17:24)
I2C: re…
Hi Biser,
is AM3358 RTC able to works at only availability of VRTC. (i.e. vddr, vdd core, vdd mpu are off)
(in short i have connect the separate 1.8v to VRTC pin at MPU and power supply TPS65217C switched off)
and
I cannot understand why this block diagram…
Please check if clocks to the GPMC module have been enabled beforehand.
hi, I am coming again. I make a new board based the starterKit board. When I try to run u-boot an the board, it stopped at the gpmc_init() int the evm.c file. In the gpmc_init() function, it stopped at this line…
Hi Arthur,
You need to include the Apache server recipe within Arago filesystem & rebuild your Arago image.
I did a google search and found some Apache bb recipes, that you could use:
http://layers.openembedded.org/layerindex/recipe/5976/
http…
Hi Biser,
Thank you.
As you know there is no part number as "AM3358ZCZ".
I am guessing it would be AM3358BZCZ80 or AM3358BZCZ100.
Best Regards
kummi
Hi Arthur,
I will forward this to the SW team.
Both the GP EVM and Starter Kit should be with AM3358ZCZ processor installed.