Tool/software:
Can't connect A8 core after Linux launched up, lower down TCLK from 10MHz to 1Mhz, 0.1MHz already.
Other cores can connect always, A8 can connect in UBOOT.
I remember I connected it and no need additional steps…
Tool/software:
Can't connect A8 core after Linux launched up, lower down TCLK from 10MHz to 1Mhz, 0.1MHz already.
Other cores can connect always, A8 can connect in UBOOT.
I remember I connected it and no need additional steps…
Tool/software:
Hi,
we are making a AM3358BZCZA100 based board with Beaglebone black as reference.
The reference design has 4GB of eMMC storage.
We are being suggested by our supplier to not use 4/8GB and go for 32GB storage for long…
Tool/software:
I am using EDMA in BeagleBone Black (am335x) for data trasnfer from source (0x4A310000) to destination (0x4A310100). Whenever I try to send 0x3457 from source, I get 0x0 at destination. How to resolve this error in…
Tool/software:
Hi,
I have a similar issue as:
Tool/software:
Hello,
I have been reading and it seems there is a way to send ADC data to a UART for transmission (reading/writing) but it has to do with No RTOS and/or the MSP line.
I am dealing with the am3358 and I wanted to…
Tool/software:
Hi there,
I am currently developing a bare metal os for the am335 processor. After some time I finally got the timer working on the dmtimer2 module. But when using the dmtimer3 module, i get a data abort with the FS…
Tool/software:
Customer plan to upgrade from SDK6(year 2012) to latest SDK9.03.
#1. Would like to keep using the old U-boot 2012, launch up Kernel fail as log, is it possible to use it in this way?
Tool/software:
I remember GPMC NOR boot was removed from SDK since v5.x, but I can't find the source.
#1. But it is still supported in user guide, but did not find the configuration of am335x_evm_nor_config / am335x_evm_norboo…
Tool/software:
I am working on DMA transfer in BB Black using PRU. This code is provided in pru software support package for am335x (BB Black).
#include <stdint.h> #include <pru_cfg.h> volatile register uint32_t __R30; volatile…
Tool/software:
I am working on BeagleBone black.
I want to acquire data at a sampling rate (10 kHz) using the inbuilt ADC of BB Black. I want to use PRU and DMA of BB Black. I don't know how to use DMA.
How to use PRU_edmaConfig…
Tool/software:
Hello,
I have a customer who uses an FPGA as the main processor and is interested in something that can serve as a USBTMC device peripheral or as an IEEE-488 device. They currently use the FX2 (CY7C68013A) from Cypress…
Tool/software:
tony@ubuntu22:~/ti-processor-sdk-linux-am335x-evm-09.03.05.02$ make linux
=====================================
Building the Linux Kernel DTBs
=====================================
make -C /home/tony/ti-processor-sdk-linux…
Tool/software:
HI there,
I'm currently developing a bare metal OS for my final highschool project. I currently have some issues with setting the DMTIMER2 module.
The Interrupt seems to fire, but when trying to use the wait function…
Tool/software:
I was trying to follow this step by step instruction for generating the example projects, and when I tried to run pdkProjectCreate.bat K2G... I constantly get the error "the system cannot find the path specified".…
Tool/software:
I am using this part to power AM3358BZCZA100 processor (Taking reference from Bealgebone)
My power input configuration is:
1. 5V input from DC supply.
2. No battery
3. No USB power
Is the schematic correct for this…
Tool/software:
Dear team,
My customer bought TMDSSK3358 from ti.com. (I am confirming the order# and when they bought) and found some difference vs. what ti.com shows.
Please check…
Tool/software:
Hi everyone,
I am new to microprocessors, Linux and networking so I need your help for my project.
I have this device with an AM3358 processor that I would like to use as a DANP device. It has two ethernet ports and…
Tool/software: Starterware
There is a strange question from customer, When USB Host is detached, write a packet of data to endpoint FIFO, will it generate abnormal interrupt like of time out, NAK, etc?
They were using Starterware…
Tool/software:
Tool/software:
Hi,
Plesae advsie if there are any document to describe the life of the TI AM3354, like as the work life or Storage life, thanks.