Browse By Tags

  • AM3358: Suggest suitable JTAG Emulators

    Part Number: AM3358
    Other Parts Discussed in Thread: SEGGER

    Hi,

    We need to use AM3358 for a new hardware design.

    We currently have XDS510 Emulator with us. Will it work with the processor? It is a 14 Pin JTAG, and the EVK of AM3358 shows 20 Pin JTAG connector…

  • AM3358: BBone Can't Receive Data from SPI0/D0

    Part Number: AM3358

    Ubuntu 18.04

    SDK 7.03

    Test Platform  : BBone Black SPI0 <---> Aardvark(SPI Tool)

    App : spidev_test.c

    I run spidev_test.(REF : 3.2.4.12. SPI — Processor SDK Linux for AM335X Documentation/

    Aardvark(SPI Tool) can receive f…

  • AM3358: AM3358: am3358/add spi device tree/run spidev_test

    Part Number: AM3358

    I follow this user guide and try to test spi function.

    3.2.4.12. SPI — Processor SDK Linux for AM335X Documentation

    spi device tree is added in file "arch/arm/boot/dts/am335x-boneblack.dts" as shown below.

    --------…
  • AM5728: Pinmux Doubt

    Part Number: AM5728
    Other Parts Discussed in Thread: AM3358,

    Hi team,

        I have doubts about Pinmux in am5728. I have also worked on the am3358 processor. In am3358 Pinmux is done in the device tree but In am5728 why is Pinmuxing done in U-boot?

    Thanks…

  • AM3358-EP: SDK 9.01 file system slow boot

    Part Number: AM3358-EP

    I am using tisdk-tiny-image-am335x-evm.tar.xz for my file system. In Ti SDK 08.02.00.24 my processor boot time was under 10 seconds. After upgrading to sdk 09.01.00.001, I am trying to use  tisdk-tiny-image-am335x-evm.tar.xz given with…

  • AM3358: am3358/add spi device tree

    Part Number: AM3358
    Other Parts Discussed in Thread: SYSCONFIG

    I follow this user guide and try to test spi function.

    3.2.4.12. SPI — Processor SDK Linux for AM335X Documentation

    spi device tree is added in file "arch/arm/boot/dts/am335x-boneblack…

  • Interrupt from PRU1 to ARM linux kernel module

    Part Number: AM3358

    I have a problem sending an interrupt from PRU to linux kernel module
    on a am335. I tried on beaglebone with TI debian and bullseye images.
    Any help would be appreciated as i'm stuck...

    Context: A fairly common and simple scenario…

  • ADC3542: appropriate MCU for high speed communication with ADC

    Part Number: ADC3542
    Other Parts Discussed in Thread: AM3358, , AM2634

    What microcontroller is suitable to communicate with ADC3542 at >10 Msps? I think the MCU should have a communication speed that is at least 100 Mbps (preferably 150Mbps). No MSP can…

  • AM3358: U-Boot Board Port 'u-boot' failed

    Part Number: AM3358

    Hi Champs,

    I'm trying to follow the steps in link below:

    https://software-dl.ti.com/processor-sdk-linux-rt/esd/AM335X/09_01_00_001/exports/docs/linux/How_to_Guides/Board_Port/U-Boot.html#overview

    to build the u-boot for a custom…

  • AM3358: SYS_RESETn pin always low despite good power supply to the MCU

    Part Number: AM3358
    Other Parts Discussed in Thread: TPS65217, , SN74LVC1G07

    Hi,

    I am bringing up a new board based on the Beagle Bone Green Wireless (BBGW). The power rails are all as expected but the MCU does not want to boot from the uSD card interface…

  • AM3358: [meta-ti] scarthgap core-image-weston

    Part Number: AM3358

    I'm working on a bringup for meta-flutter on the beaglebone black DRM backend.


    First pass is with core-image-weston.  Weston fails to initialize with:

    Mar 30 09:44:24 beaglebone weston[490]: [09:44:24.-1097469832] EGL error state…
  • AM3358: AM33x TICLICD linux clarification DPI to LVDS converter

    Part Number: AM3358
    Other Parts Discussed in Thread: SN65LVDS84A
    Hello !

    So, I'm trying to integrate a LVDS panel via the SN65LVDS84A .
    According to TI , currently the way to integrate a new panel is to make use of the TILCDC linux driver . 
    This driver…
  • [FAQ] AM6x: Latest FAQs on AM62x, AM64x, AM24x, AM3x, AM4x Sitara devices

  • AM3358: AM335x BeagleBone Black and TPM SLB9670 communication issue

    Part Number: AM3358

    Hi,
    I get this error when trying to interface SLB9670 with BeagleBone Balck over SPI1, bus with CS1:

    tpm_tis_spi: probe of spi1.1 failed with error -110

    This is my overlay:

    /dts-v1/;
    /plugin/;

    / {
    compatible = "ti,beaglebone","ti,am335x…

  • AM3358: Having TI load the Debian OS so we can eliminate the SD Card connector from our PCB design.

    Part Number: AM3358
    Other Parts Discussed in Thread: UNIFLASH

    Hello all,

    We wish to have TI load the Debian OS into the AM3358BZCZA100 so we can eliminate the SD Card connector from our PCB design.

    Please let me know if you can do this.  I'm aware that…

  • AM3358: Is it possible to load initialized data into PRU_SHAREDMEM using linker placement?

    Part Number: AM3358

    Hi all,

    On a project I'm working on, the AM3358 PRU drives a led display and the image data is kept in the shared RAM.

    I am experimenting with the linker script to attempt to load an initial display image which should be loaded…

  • AM3358: Ethernet PHY MDIO access

    Part Number: AM3358

    Hi,

    The BBB board has a LAN8710A PHY connected to the processor AM3358. I'm trying to access the Ethernet PHY register available on BeagleBone Black board. I am not using so I want to disable this PHY, ultimately some power will…

  • AM3358: Gigabit Ethernet with the AM335x

    Part Number: AM3358
    Other Parts Discussed in Thread: AM3357

    Hi,

    Q1. I'm considering using Gigabit Ethernet with the AM335x. Am I correct in my understanding that if I want to perform 1 Gigabit communication with AM335x, I need to use a model number with…

  • AM2632: PRU eGPI and eGPO Mapping to Pins at Device Level

    Part Number: AM2632
    Other Parts Discussed in Thread: AM3358

    Hi,

    I have a question about routing the eGPI and eGPO to the device-level pins. According to the Datasheet, the PR0_PRUn_GPIO mode can be configured for a pin at a device level, however I couldn…

  • AM2632: PRP Ethernet

    Part Number: AM2632
    Other Parts Discussed in Thread: AM3356, AM3357, AM3358, AM3359, AM4376, AM4377, AM4378, AM4379, AM5716, AM5718, AM5726, AM5728, AM5746, AM5748, AM5749, AM6548, AMIC110

    Does the PRU-ICSS on the AM2632 support PRP ethernet mode?

    I see…

  • AM3358: AM335x accidental Unable to mount UBI file system from nand flash, and cannot be automatically restored after it appears.

    Part Number: AM3358
    Other Parts Discussed in Thread: DA8XX, TPS65910

    Hello everyone,

    The previous file system saved on the SD card may be damaged, so a backup plan is proposed to backup some important data from the SD card to flash, and the file system…

  • AM3358: USB communication:

    Part Number: AM3358

    During bulk transfer mode some packet get lost on call of USBBufferWrite(const tUSBBuffer *psBuffer, const unsigned char *pucData,
    unsigned int ulLength) function.

  • AM3358: Compatibility Issue with MK27 EMMC on BBB Between Kernel Versions 6.10 and 4.19

    Part Number: AM3358

    On the linux kernel version 6.1.x, users have reported a significant issue with the MK27 EMMC on BBB, leading to its malfunction and eventual damage. However, intriguingly, this problem seems to be non-existent when using kernel version…

  • AM3358: bitbake -k tisdk-default-image fails to apply patch '0001-tests-Allow-different-output-from-mv.patch'

    Part Number: AM3358

    Hi,

    I'm trying to build an arago yocto distro for my am335x board, but it fails immediately.

    I'm following https://software-dl.ti.com/processor-sdk-linux/esd/AM335X/09_01_00_001/exports/docs/linux/Overview_Building_the_SDK…

  • AM3359: GPIO Direction Configuration Issue: default value is low

    Part Number: AM3359

    Hi TI team,

    I am facing an issue while defining the GPIO direction as output. I am using GPIO2_5 as the LAN PHY reset, which is one of the inputs of the 7UL1T80FU AND logic IC. This pin operates at 1.8V, while the second input and…

« 3 4 5 6 7 »