Browse By Tags

  • ADS7961-Q1: ADC Recommendation

    Part Number: ADS7961-Q1
    Other Parts Discussed in Thread: ADS8661, TIC12400-Q1, TMUX1308, TMUX1308-Q1, ADS8665, MUX36S08, ADS7961

    Tool/software:

    Hi team, 

    Customer is looking for a 16 channel ADC with SPI interface. They don't have strict requirement for…

  • MUX36S08: MUX36S08IPW Mux IC failed, Resistance change observed across Pin 8 and Gnd Pin

    Part Number: MUX36S08
    Other Parts Discussed in Thread: TMUX7308F

    Hello Team,

    We are using MUX36S08IPW muxer for our 4-20mA Sensor.

    We have 2 ICs failed with various condition.

    Condition 1: 

    The resistance across the Pin 8 and GND was showing 1.8k.

    Condition…

  • CD4051B: Control signal falling edge spikes on output signal.

    Part Number: CD4051B
    Other Parts Discussed in Thread: MUX36S08

    Hello, I am getting spikes on the output of a CD4051BM that appear to be inductive feedthrough from the control signals:

    Top trace is the pin13 output, bottom trace is the A control signal…

  • MPC508: MPC508AU/1K glitch issue Charge Injection

    Part Number: MPC508
    Other Parts Discussed in Thread: OPA2277, TMUX4051, MUX36S08, MUX508, TMUX7308F, , DAC8820

    Hi,

     We are using DAC8820ICDBR part in our design that provides boipolar output(+/-10V). The connections are given as recommended in datasheet…

  • MUX36S08EVM-PDK: Parameters and attenuation issues.

    Part Number: MUX36S08EVM-PDK
    Other Parts Discussed in Thread: MUX36S08, MUX508, TMUX1308-Q1, SN74CBTLV3253, SN74CBTLV3251, TMUX1309-Q1

    Hi all, 

    1. The bandwidth on the MUX36S08 datasheet shows 500MHZ, Not sure what this figure means about, on datasheet…

  • TMUX4051: Appropriate MUX for shut register

    Part Number: TMUX4051
    Other Parts Discussed in Thread: TMUX4052, , MUX506, MUX36S16, MUX36S08, TMUX1072, INA186, TMUX7208

    Dear Technical Support Team,

    I'd like to configure 32:1+EN (output Hi-Z) using multiple MUX.
    TMUX4051 and TMUX4052 are especially…

  • MUX508: SPICE Model file describes MUX36S08 and MUX36D04 instead of MUX508

    Part Number: MUX508
    Other Parts Discussed in Thread: MUX36D04, , MUX36S08, TINA-TI

    The MUX508 product page has a TINA-TI Spice Model available for download. When I download the .TSM file and open the macro in TINA-TI, it looks like the subcircuit describes…

  • [FAQ] What is Charge Injection?

    Other Parts Discussed in Thread: MUX36S08

    What is Charge Injection?

    Charge injection (QINJ) is the coupling of the switch control signal through some parasitic capacitance. The charge present from this parasitic capacitance is then injected into the switch…

  • MUX36S08: Is there any device p2p compatible with ADG1608BCP?

    Part Number: MUX36S08
    Other Parts Discussed in Thread: TMUX6208, TMUX1108

    Hi,

    is there any device have same package with ADG1608BCP? Thx

  • [FAQ] Multiplexers and Switches Selection Guide | Mid Voltage Mux 25V =< VSIGNAL =< 99V

    The following table helps select the right multiplexer and switch with Mid Voltage 25V =< VSIGNAL =< 99V in different configurations:


    Precision,
     Protection, Automotive, Extended Temperature

     

    Configuration

    16:1

    MUX36S16

    MUX506

  • MUX36S08: Need information

    Part Number: MUX36S08

    Hi Team,

    May I ask for help? Our customer have concerns as shown below:
    "I working in a semiconductor company i need the below information of IC(MUX36S08IRRJR ). These information is not listed in data sheet."

    • Digital input…
  • MUX36S08: WQFN package difference

    Part Number: MUX36S08

    Hello team,

    Could you let me know why we have two package options(RUM and RRJ) for WQFN of MUX36S08?

    Which do you recommend in terms of delivery?

    Best regards,

  • MPC508: single supply

    Part Number: MPC508
    Other Parts Discussed in Thread: MUX36S08, TMUX7208

    Hi Team,

    Can this device to work in single supply voltage?

    If yes, any performance difference?

    Also, how is digital input VIL/VIH?

    Thanks! 

    Andrew

  • RE: TMUX1309: Confirm if the design is reliable for continuous operation

    Hi Jonathan,

    Thank you for reaching out. 

    The functional use of the 8:1 Mux to sample the 8 input signals one at a time looks good as it will save lot of component space/cost. They need to account for the switch RON/RDSon resistance in the calculation…

  • RE: MUX36S08EVM-PDK: How to power and use MUX36S08EVM

    Hey Minrak, 

    The datasheet for the MUX36S08 actually shows performance using single sided and dual supply. You'll see the parameters tested at the top of the electrical characteristics section (Looks like 7.5 is dual and 7.6 is single). 
    You'll see…

  • RE: Reg: Developing high side switch for 20uA continuous current.

    Hey S.P

    My understanding is that you have a 17V signal with a current of 20uA. Now what happens next is where you lost me a little bit.But i'm understanding that you need a enable Low device who's logic level are Vih = 3V and is a 1:1 switch to connect…

  • RE: TMUX6136: Rds on 120 Ω

    Hi Alex,


    All Parameters in TAN refer to Recommended Operating Conditions and/or Absolute Maximums.

    Due to the differences in power supply ranges and available data we have parameters in PINK referring to the 12V single supply table, the only comparable…

  • RE: TDC1000-C2000EVM: Multiplexer module for

    Hi Minrak,

    Responding to your questions in order:

    1) The MUX36 part numbers are offered specifically for the PGA460 because the direct-driver of the PGA460 can reach upward of 30V. In the case of the TDC1000, the driver voltage is limited to 5V, so the…

  • TDC1000-C2000EVM: Multiplexer module for

    Part Number: TDC1000-C2000EVM

    Hello.

    Once I asked about how to multiplex the TDC1000-C2000 EVM. Please refer to the forum discussed before 
    (https://e2e.ti.com/support/sensors/f/1023/t/603257).

     1. First of all, the engineer in the form says I have to make…

  • RE: TIDA-01471: Multiplexers and current source based on TLV431BQ

    Hi Victor,

    1. You are right, using general MUX61xxx was an oversight. Only TMUX6104 can support 36V.

    You can select one of the following list based on the number of channels.

  • TIDA-01471: Multiplexers and current source based on TLV431BQ

    Part Number: TIDA-01471
    Other Parts Discussed in Thread: MUX36S08, TMUX6104

    Dear Ahmed,

    I have two questions related to this reference design.

    1. In this forum thread, you mentioned the preferred multiplexer for the current source: MUX36xxx or MUX61xxx…

  • RE: MUX36S08: On capacitance influence on Settling behavior

    Hi Rock Su,

    Thank you for sharing the TI precision lab Mux videos with the customers and sharing the feedback with us.

     " K "is the number of time constants required to settle an N bit accurate system". It is referring to computing how many…

  • MUX36S08: On capacitance influence on Settling behavior

    Part Number: MUX36S08

    Dear colleague,

    Now we are promoting TI precision lab MUX video to customers.

    But in Con as below:

    What does K mean? In video, it means that "where K is the number of time constants required to settle an N bit accurate system"…

  • RE: WEBENCH® Tools/MUX36S08: I required PSPICE model for MUX36S08

    Hi Rajani,

    The SPICE model for MUX36S08 is attached, which was extracted from the TINA netlist.

    MUX36SO8 SPICE.zip

    Best regards,

    Kate

  • RE: WEBENCH® Tools/MUX36S08: I required PSPICE model for MUX36S08

    Hi Rajani,

    Thanks for your request! Our team is looking into getting this model for you. I will update you soon. 

    Regards,

    Kate

1 2 3