In the datasheet for the LM293 and other variants of this comparator, Section 7.3 states:
The output NPN will sink current when the positive input voltage is higher than the negative input voltage and the offset voltage.
In the same datasheet, section 8.2.2.1 states:
If IN- is higher than IN+ and the offset voltage, the output is low and the output transistor is sinking current
I find this odd. And by 'odd', I mean really conflicting.
Please explain.