Will the LMH6655 be damaged if the + input is driven (voltage follower configuration) with any voltage and both power pins are not connected to power? I believe it will not be damaged because there is no current path to ground or supply.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Will the LMH6655 be damaged if the + input is driven (voltage follower configuration) with any voltage and both power pins are not connected to power? I believe it will not be damaged because there is no current path to ground or supply.
Hi Dave,
I've not tested the LMH6655 this way, but I also tend to agree with you that this should not damage the device.
Have you encountered a failure this way?
Regards,
Hooman
I want to power down some of these devices to save power but have a driven signal into the + input of the part. Do you know if there is a current limit in this condition where the power supply is attached to the part but the supplies are not on?
Thanks, Dave