We have designed and built a test circuit and a PCB for an application we are developing using the XTR111 (see attachments).
After a damaged mosfet BSP171 we replaced it with a different (but similar?) BSP315 which we could find in time.
Our MCU has an Aout 0-3.22v (measured value) @ 12bit resolution, and the XTR111 is powered with 12vdc.
During my first test for linearity (see attachment for test values) at around 0.80v Vin the output drifted rapidly (0.5mA/sec) to a max of 33.3mA.
That did happen before but with much lower rate and much lower Imax at the end (1mA offset from the expected value), and when I changed the Vin it did get back to normal values.
Now at 0Vin the Iout is around 16~19mA (very unstable) and at around 0.7V goes to the max value of 33.3mA (very unstable 30~33.3mA)
Question: What's wrong!
Schematic: XTR111 4-20mA.pdf
PCB Layout:XTR111 4-20mA PCB.pdf
First linearity test:Linearity Test 31Aug2015.xls