Hi,
We can program clk outputs 1Ghz to 2.4 Ghz but, we have no clk output less then 800 Mhz.
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
We can program clk outputs 1Ghz to 2.4 Ghz but, we have no clk output less then 800 Mhz.
Thanks
R0 (INIT) 0x000090 R0 0x000010 R2 0x000200 R256 0x010003 R257 0x010155 R259 0x010301 R260 0x010402 R261 0x010500 R262 0x0106F1 R263 0x010700 R264 0x01080C R265 0x010955 R267 0x010B00 R268 0x010C02 R269 0x010D00 R270 0x010EF1 R271 0x010F00 R272 0x011001 R273 0x011155 R275 0x011300 R276 0x011402 R277 0x011500 R278 0x0116F9 R279 0x011710 R280 0x011801 R281 0x011955 R283 0x011B00 R284 0x011C02 R285 0x011D00 R286 0x011EF9 R287 0x011F01 R288 0x01200C R289 0x012155 R291 0x012300 R292 0x012402 R293 0x012500 R294 0x0126F9 R295 0x012711 R296 0x012808 R297 0x012955 R299 0x012B00 R300 0x012C02 R301 0x012D00 R302 0x012EF9 R303 0x012F00 R304 0x013018 R305 0x013155 R307 0x013301 R308 0x013402 R309 0x013500 R310 0x0136F1 R311 0x013711 R312 0x013805 R313 0x013900 R314 0x013A0C R315 0x013B00 R316 0x013C00 R317 0x013D08 R318 0x013E03 R319 0x013F00 R320 0x01400F R321 0x014100 R322 0x014200 R323 0x014331 R324 0x014400 R325 0x01457F R326 0x014618 R327 0x01471A R328 0x014802 R329 0x014942 R330 0x014A02 R331 0x014B16 R332 0x014C00 R333 0x014D00 R334 0x014EC0 R335 0x014F7F R336 0x015003 R337 0x015102 R338 0x015200 R339 0x015300 R340 0x015478 R341 0x015500 R342 0x015678 R343 0x015700 R344 0x015896 R345 0x015904 R346 0x015AB0 R347 0x015BD4 R348 0x015C20 R349 0x015D00 R350 0x015E00 R351 0x015F0C R352 0x016000 R353 0x016101 R354 0x016244 R355 0x016300 R356 0x016400 R357 0x01650C R380 0x017C15 R381 0x017D33 R358 0x016600 R359 0x016700 R360 0x01680C R361 0x016959 R362 0x016A20 R363 0x016B00 R364 0x016C00 R365 0x016D00 R366 0x016E14 R371 0x017300 R8189 0x1FFD00 R8190 0x1FFE00 R8191 0x1FFF53
R0 (INIT) 0x000090 R0 0x000010 R2 0x000200 R256 0x010003 R257 0x010155 R259 0x010301 R260 0x010402 R261 0x010500 R262 0x0106F1 R263 0x010700 R264 0x01080C R265 0x010955 R267 0x010B00 R268 0x010C02 R269 0x010D00 R270 0x010EF1 R271 0x010F00 R272 0x011001 R273 0x011155 R275 0x011300 R276 0x011402 R277 0x011500 R278 0x0116F9 R279 0x011710 R280 0x011801 R281 0x011955 R283 0x011B00 R284 0x011C02 R285 0x011D00 R286 0x011EF9 R287 0x011F01 R288 0x01200C R289 0x012155 R291 0x012300 R292 0x012402 R293 0x012500 R294 0x0126F9 R295 0x012711 R296 0x012808 R297 0x012955 R299 0x012B00 R300 0x012C02 R301 0x012D00 R302 0x012EF9 R303 0x012F00 R304 0x013018 R305 0x013155 R307 0x013302 R308 0x013402 R309 0x013500 R310 0x0136F1 R311 0x013711 R312 0x013805 R313 0x013900 R314 0x013A0C R315 0x013B00 R316 0x013C00 R317 0x013D08 R318 0x013E03 R319 0x013F00 R320 0x01400F R321 0x014100 R322 0x014200 R323 0x014331 R324 0x014400 R325 0x01457F R326 0x014618 R327 0x01471A R328 0x014802 R329 0x014942 R330 0x014A02 R331 0x014B16 R332 0x014C00 R333 0x014D00 R334 0x014EC0 R335 0x014F7F R336 0x015003 R337 0x015102 R338 0x015200 R339 0x015300 R340 0x015478 R341 0x015500 R342 0x015678 R343 0x015700 R344 0x015896 R345 0x015904 R346 0x015AB0 R347 0x015BD4 R348 0x015C20 R349 0x015D00 R350 0x015E00 R351 0x015F0C R352 0x016000 R353 0x016101 R354 0x016244 R355 0x016300 R356 0x016400 R357 0x01650C R380 0x017C15 R381 0x017D33 R358 0x016600 R359 0x016700 R360 0x01680C R361 0x016959 R362 0x016A20 R363 0x016B00 R364 0x016C00 R365 0x016D00 R366 0x016E14 R371 0x017300 R8189 0x1FFD00 R8190 0x1FFE00 R8191 0x1FFF53
I attached 2 files. 2.4GHz and 100 MHz configurations. I can observe 2.4 GHz clock signal but cant 100 MHz. I use same port. Also I have tried other ports for same files, result is same. 2.4 GHz configurations run in Bypass mode.
In our design there are 6 clock outputs (not sysref) Whenever I use bypass mode for all of them I can observe 2.4GHz clk . For higher division values I couldn't observe.