This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

CDCLVD2102: Is the CDCLVD2102 recommended/suitable for driving LVDS over a long backplane?

Prodigy 10 points

Replies: 1

Views: 145

Part Number: CDCLVD2102

Hi, 

I understand from the datasheet that the CDCLVD2102 is suitable for driving 100 ohm differential loads with its differential LVDS outputs. I would like to know if TI considers this part suitable to drive LVDS pairs over a long backplane (perhaps on the order of 15 inches) or would recommend it for such a purpose. 

Thanks

  • CDCLVC2102 should be suitable for these requirements. I have seen issues driving transmission lines that are several meters long, but to be on the safe side, I recommend to simulate it. You can download the IBIS model here: www.ti.com/.../toolssoftware

    Kind regards,
    Lane

    ____________________________________________________________________________________

    To design your own Clock Tree solution, visit WEBENCH Clock Architect ​​​​

    More information Clock and Timing System products: http://www.ti.com/clock-and-timing/overview.html

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.