Other Parts Discussed in Thread: CDCM6208
Hi Dear
The configuration of the device CDCM6208V1F is:
reg0: 01B9
reg1: 000C
reg2: 0017
reg3: 10F0
reg4: 234D
reg5: 01BB
reg6: 0002
reg7: 0023
reg8: 0005
reg9: 0003
reg10: 0050
reg11: 0000
reg12: 0003
reg13:0050
reg14:0000
reg15:00D3
reg16:0170
reg17:0000
reg18:00D3
reg19:0170
reg20:0000
My whole design is like the following picture:
register0~20 reading value is the same with the value I want to write.
But reg21.1 = 1 which means Loss of ireference input. I use an active crystal as the refference input, frequency is 100MHz, 3.3V LVDS and I'm sure that the crystal is ok.
Could you please help me analysis this issue? Is the configuration right?