Hello,
I am developing a system that uses LMK61E2BAA as main oscillator. I am using TI provided Oscillator Programming tool for generation of register maps, however, even while tool reports that target frequency is achieved with 0ppm error, actual output frequency is much higher that desired one. For example, when I attempt to set 196.608MHz output, i measure 198.826MHz in circuit.
I am performing measurements using built in frequency counter function of Keysight MSOX3054T with have specified much lower maximum error. I have compared my measurements to several known-good fixed oscillators to rule out measurement error, but they provided perfectly valid readings.
No matter what frequency i attempt to set on LMK, i always get frequency larger by slightly more than 1%. This is much larger that advertised maximum of +-50ppm total error.
However, when i measure output with factory programmed configuration,the default frequency (156.25MHz) is properly generated with 0.00134% error.
Can anyone suggest what is the reason of such situation?
For reference, i have attached below register map generated by TI tool.
Best regards.
R0 0x0010 R1 0x010B R2 0x0233 R8 0x08B0 R9 0x0901 R16 0x1000 R17 0x1180 R21 0x1502 R22 0x1600 R23 0x171C R25 0x1900 R26 0x1A37 R27 0x1B00 R28 0x1C07 R29 0x1D73 R30 0x1E00 R31 0x1F0C R32 0x2035 R33 0x2103 R34 0x2224 R35 0x2327 R36 0x2412 R37 0x2502 R38 0x2602 R39 0x2707 R47 0x2F00 R48 0x3000 R49 0x3110 R50 0x3200 R51 0x3300 R52 0x3400 R53 0x3500 R56 0x3800 R72 0x4802