HI,
In our application , LMX2581 differential sine wave outputs are used to drive LMK01801 inputs and the buffer divided ouputs of LMK01801 are used for DAC (data clock :108 Mhz & dacout 432 Mhz) clocks and ADC clock (108 Mhz) respectively.
The power levels in lmx2581 (OUTx_PWR ) are set to the value : 15 which is close to 4dbm ?? (resistive pullup) which are driving lmk01801 inputs . lmk01801 has been programmed via microwire but there are no ouputs.
Is the programmed power in lmx2581 is sufficient to drive the inputs of lmk01801 ?
plz explain what should be the outx_pwr in lmx2581 has to programmed so that the differential sine wave outputs can sufficiently drive the inputs of lmk01801 ?