Part Number: TDA4VEN-Q1
Other Parts Discussed in Thread: DRA821
Tool/software:
The CAN interface is not working under Linux. How can I troubleshoot this?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TDA4VEN-Q1
Other Parts Discussed in Thread: DRA821
Tool/software:
The CAN interface is not working under Linux. How can I troubleshoot this?
Updated last 2026/11/02
As an example, TDA4VEN is used, but this guide should be somewhat applicable to all TDA4x and AM6x devices using Linux. There will be differences with available interfaces, pins, and names, but overall flow is same for all device.
Check to see if MCAN driver is initialized during boot. This can be done by running the following command:
If CAN driver is being probed to be initialized, then the following logs that say "m_can device registered" will be printed:
root@j722s-evm:/opt/edgeai-gst-apps# dmesg | grep can [ 0.412218] HugeTLB: 0 KiB vmemmap can be freed for a 1.00 GiB page [ 0.425552] HugeTLB: 0 KiB vmemmap can be freed for a 32.0 MiB page [ 0.438891] HugeTLB: 0 KiB vmemmap can be freed for a 2.00 MiB page [ 0.452224] HugeTLB: 0 KiB vmemmap can be freed for a 64.0 KiB page [ 1.736111] cpu cpu0: OPP table can't be empty [ 9.172670] m_can_platform 4e18000.can: m_can device registered (irq=543, version=32) [ 9.201131] m_can_platform 20701000.can: m_can device registered (irq=544, version=32) [ 9.298068] m_can_platform 4e08000.can: m_can device registered (irq=545, version=32) [ 10.199408] m_can_platform 20701000.can main_mcan0: renamed from can1 [ 10.263624] m_can_platform 4e18000.can mcu_mcan1: renamed from can0 [ 10.345368] m_can_platform 4e08000.can mcu_mcan0: renamed from can2 root@j722s-evm:/opt/edgeai-gst-apps#
* note, above logs are from TDA4VEN TI board using the edgeai 10.1 prebuilt image.
Problem: If "m_can device registered" logs are not printing out, this indicates that the CAN driver is not probed, or it is probed but there is an error.
Solution:
1.1. If no CAN related logs are received, then most likely the devicetree does not have the CAN nodes defined.
1.2. If CAN driver is probed, but there is an error, then most likely that it is an pinmux issue. Please check the pinmux in devicetree one more time.
1.3. Alternatively, the .ko kernel module for CAN is not installed, or kernel config is wrong. Please check "lsmod" to see if kernel modules are loaded as well as "zcat /proc/config.gz" to see the kernel config. The output should be grepped, case insensitive, for "CAN" related drivers.
Run the following command to see if MCAN kernel driver is initialized:
If driver is initialized correctly, then the following logs should be outputted:
root@j722s-evm:/opt/edgeai-gst-apps# ifconfig -a
eth0: flags=4099<UP,BROADCAST,MULTICAST> mtu 1500
ether 58:a1:5f:c1:d1:09 txqueuelen 1000 (Ethernet)
RX packets 0 bytes 0 (0.0 B)
RX errors 0 dropped 0 overruns 0 frame 0
TX packets 0 bytes 0 (0.0 B)
TX errors 0 dropped 0 overruns 0 carrier 0 collisions 0
lo: flags=73<UP,LOOPBACK,RUNNING> mtu 65536
inet 127.0.0.1 netmask 255.0.0.0
inet6 ::1 prefixlen 128 scopeid 0x10<host>
loop txqueuelen 1000 (Local Loopback)
RX packets 82 bytes 6916 (6.7 KiB)
RX errors 0 dropped 0 overruns 0 frame 0
TX packets 82 bytes 6916 (6.7 KiB)
TX errors 0 dropped 0 overruns 0 carrier 0 collisions 0
main_mcan0: flags=128<NOARP> mtu 16
unspec 00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00 txqueuelen 10 (UNSPEC)
RX packets 0 bytes 0 (0.0 B)
RX errors 0 dropped 0 overruns 0 frame 0
TX packets 0 bytes 0 (0.0 B)
TX errors 0 dropped 0 overruns 0 carrier 0 collisions 0
device interrupt 32
mcu_mcan0: flags=128<NOARP> mtu 16
unspec 00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00 txqueuelen 10 (UNSPEC)
RX packets 0 bytes 0 (0.0 B)
RX errors 0 dropped 0 overruns 0 frame 0
TX packets 0 bytes 0 (0.0 B)
TX errors 0 dropped 0 overruns 0 carrier 0 collisions 0
device interrupt 33
mcu_mcan1: flags=128<NOARP> mtu 16
unspec 00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00 txqueuelen 10 (UNSPEC)
RX packets 0 bytes 0 (0.0 B)
RX errors 0 dropped 0 overruns 0 frame 0
TX packets 0 bytes 0 (0.0 B)
TX errors 0 dropped 0 overruns 0 carrier 0 collisions 0
device interrupt 31
root@j722s-evm:/opt/edgeai-gst-apps#
2.1 Problem: "ifconfig -a" does not show the CAN interfaces
Solution: Please go back to "Step 1".
Initialize and test a MCAN interface in CAN-FD loopback mode. This can be done with a single CAN instance with no extra hardware.
# Put the controller in internal loopback mode
root@j722s-evm:/opt/edgeai-gst-apps# ip link set main_mcan0 type can bitrate 1000000 dbitrate 5000000 fd on loopback on
root@j722s-evm:/opt/edgeai-gst-apps# ip link set main_mcan0 up
# Check the details for main_mcan0 node, this should show LOOPBACK
root@j722s-evm:/opt/edgeai-gst-apps# ip -details link show main_mcan0
4: main_mcan0: <NOARP,UP,LOWER_UP,ECHO> mtu 72 qdisc pfifo_fast state UP mode DEFAULT group default qlen 10
link/can promiscuity 0 allmulti 0 minmtu 0 maxmtu 0
can <LOOPBACK,FD> state ERROR-ACTIVE (berr-counter tx 0 rx 0) restart-ms 0
bitrate 1000000 sample-point 0.750
tq 12 prop-seg 29 phase-seg1 30 phase-seg2 20 sjw 10 brp 1
m_can: tseg1 2..256 tseg2 2..128 sjw 1..128 brp 1..512 brp_inc 1
dbitrate 5000000 dsample-point 0.750
dtq 12 dprop-seg 5 dphase-seg1 6 dphase-seg2 4 dsjw 2 dbrp 1
m_can: dtseg1 1..32 dtseg2 1..16 dsjw 1..16 dbrp 1..32 dbrp_inc 1
clock 80000000 numtxqueues 1 numrxqueues 1 gso_max_size 65536 gso_max_segs 65535 tso_max_size 65536 tso_max_segs 65535 gro_max_size 65536 gso_ipv4_max_size 65536 gro_ipv4_max_size 65536 parentbus platform parentdev 20701000.can
# Run candump in background
root@j722s-evm:/opt/edgeai-gst-apps# candump main_mcan0 &
[1] 1610
root@j722s-evm:/opt/edgeai-gst-apps# [ 2620.760472] can: controller area network core
[ 2620.764928] NET: Registered PF_CAN protocol family
[ 2620.780625] can: raw protocol
# Send message on main_mcan0, this should be echoed back on the console as candump is running in background
root@j722s-evm:/opt/edgeai-gst-apps# cansend main_mcan0 113##2AAAAAAAA
main_mcan0 113 [04] AA AA AA AA
main_mcan0 113 [04] AA AA AA AA
root@j722s-evm:/opt/edgeai-gst-apps#
3.1 Problem:
Wrong CAN-frame format!
root@j722s-evm:/opt/edgeai-gst-apps# cansend main_mcan0 113##2AAAAAAAAA
Wrong CAN-frame format!
cansend - send CAN-frames via CAN_RAW sockets.
Usage: cansend <device> <can_frame>.
<can_frame>:
<can_id>#{data} for Classical CAN 2.0 data frames
<can_id>#R{len} for Classical CAN 2.0 data frames
<can_id>#{data}_{dlc} for Classical CAN 2.0 data frames
<can_id>#R{len}_{dlc} for Classical CAN 2.0 data frames
<can_id>##<flags>{data} for CAN FD frames
<can_id>:
3 (SFF) or 8 (EFF) hex chars
{data}:
0..8 (0..64 CAN FD) ASCII hex-values (optionally separated by '.')
{len}:
an optional 0..8 value as RTR frames can contain a valid dlc field
_{dlc}:
an optional 9..F data length code value when payload length is 8
<flags>:
a single ASCII Hex value (0 .. F) which defines canfd_frame.flags
Examples:
5A1#11.2233.44556677.88 / 123#DEADBEEF / 5AA# / 123##1 / 213##311223344 /
1F334455#1122334455667788_B / 123#R / 00000123#R3 / 333#R8_E
root@j722s-evm:/opt/edgeai-gst-apps#
Solution: CAN-FD supports a flexible message payload, but when using the Linux CAN utility tools, the messages should be sent in multiples of 8 bits or 2 hex characters.
3.2 Problem: The "ip link set" command does not work
Solution: Most likely the CAN driver is not initialized. Please go to "Step 1" in the troubleshooting guide. Otherwise, it may be different name for the interface (for example, instead of main_mcan0, might be can0).
3.3 Problem: No data is being received or sent
Solution: Please make sure the "candump" command is running in the background. This may be checked using "ps aux | grep can" to get below logs that candump is running.
root@j722s-evm:/opt/edgeai-gst-apps# ps aux | grep can root 565 0.0 0.0 2888 1408 ? Ss 18:44 0:00 /usr/sbin/tee-supplicant root 1675 0.0 0.0 2076 896 ttyS2 S 20:12 0:00 candump main_mcan0 root 1677 0.0 0.0 3496 1280 ttyS2 S+ 20:12 0:00 grep can root@j722s-evm:/opt/edgeai-gst-apps#
Can run same exact commands on a different Linux device (like a PC) or an external loopback connecting two CAN instances on the EVM, since all the Jacinto7 TI EVM has multiple CAN instances pinned out. Other OS also works, as long as the configurations match between sender/receiver.
To see which pins are for CAN, please check EVM user guide. The guides are available from the respective EVM purchase page:
https://www.ti.com/tool/J722SXH01EVM
Specifically, this page is the EVM user guide:

Details for CAN connection are also on the same EVM user guide:

On receiver, set up CAN-FD and candump like below:
# Initialize CAN-FD
root@j722s-evm:/opt/edgeai-gst-apps# ip link set main_mcan0 type can bitrate 1000000 dbitrate 5000000 fd on
root@j722s-evm:/opt/edgeai-gst-apps# ip link set main_mcan0 up
# Check the details for main_mcan0 node
root@j722s-evm:/opt/edgeai-gst-apps# ip -details link show main_mcan0
4: main_mcan0: <NOARP,UP,LOWER_UP,ECHO> mtu 72 qdisc pfifo_fast state UP mode DEFAULT group default qlen 10
link/can promiscuity 0 allmulti 0 minmtu 0 maxmtu 0
can <LOOPBACK,FD> state ERROR-ACTIVE (berr-counter tx 0 rx 0) restart-ms 0
bitrate 1000000 sample-point 0.750
tq 12 prop-seg 29 phase-seg1 30 phase-seg2 20 sjw 10 brp 1
m_can: tseg1 2..256 tseg2 2..128 sjw 1..128 brp 1..512 brp_inc 1
dbitrate 5000000 dsample-point 0.750
dtq 12 dprop-seg 5 dphase-seg1 6 dphase-seg2 4 dsjw 2 dbrp 1
m_can: dtseg1 1..32 dtseg2 1..16 dsjw 1..16 dbrp 1..32 dbrp_inc 1
clock 80000000 numtxqueues 1 numrxqueues 1 gso_max_size 65536 gso_max_segs 65535 tso_max_size 65536 tso_max_segs 65535 gro_max_size 65536 gso_ipv4_max_size 65536 gro_ipv4_max_size 65536 parentbus platform parentdev 20701000.can
# Run candump
root@j722s-evm:/opt/edgeai-gst-apps# candump main_mcan0
[1] 1610
root@j722s-evm:/opt/edgeai-gst-apps# [ 2620.760472] can: controller area network core
[ 2620.764928] NET: Registered PF_CAN protocol family
[ 2620.780625] can: raw protocol
For sender, do similar set up, but use cansend for last command
4.1 Problem: The "ip link set" command does not work
Solution: Most likely the CAN driver is not initialized. Please go to "Step 1" in the troubleshooting guide. Otherwise, it may be different name for the interface (for example, instead of main_mcan0, might be can0).
4.2 Problem: "Protocol error in Arbitration fail" and or "Data phase error detected" is printed out
Solution:
4.3 Problem: m_can_platform 2731000.can main_mcan3: bus-off
Solution: For J7200/DRA821 before 6.6 kernel, this was a known issue and this commit can fix: https://git.ti.com/cgit/ti-linux-kernel/ti-linux-kernel/commit/arch/arm64/boot/dts/ti/k3-j7200-som-p0.dtsi?h=ti-linux-6.6.y&id=5552de2bfa63a4a6e84c102a50f50ae517725007
For other cases, it could be the transceiver nodes in device tree are not configured correctly: https://git.ti.com/cgit/ti-linux-kernel/ti-linux-kernel/tree/arch/arm64/boot/dts/ti/k3-j721e-sk.dts?h=ti-linux-6.6.y#n222
4.4 Problem: Data is not going out.
Solution:
Please post a new E2E forum post and share details of the issue at hand, along with the full output from "dmesg".
Regards,
Takuma
Last updated 2026/07/22.
https://www.ti.com/lit/pdf/spradp4
J722S Linux example: https://software-dl.ti.com/jacinto7/esd/processor-sdk-linux-j722s/11_02_01_03/exports/docs/linux/Foundational_Components/Kernel/Kernel_Drivers/MCAN.html
Regards,
Takuma