I also have a lot of problems running transient, get kind of random results depending on time length, not sure - the V7 version of the RC4558 is attached 4213.AcerbergMossbert BP with RC4558 25kHz redesign 4th order.TSC
The CAN module will not receive its own message unless loopback mode has been set. Unfortunately there is no TivaWare function to do that. Here is the code I used to set that mode. I have attached a simple CCS project example as well.
// Enable loopback…
Hi Lane,
I have installed the 4213.Driver_ProgrammingEVM_Windows7.zip driver and the device manager shows the EVM can be identified, which is shown below.
But the device still can’t be detected. The phenomenon is below. If the device is identified…
Part Number: MSP-EXP430F5529LP Other Parts Discussed in Thread: CCSTUDIO , MSP430FR5969 , MSP430F5500 OK - I'm unable to install CSS Studio it gives the error:
[15:39:22] CCS_INFO: Installing feature com.ti.ccstudio.installer.linux64.feature.group Executing…
Part Number: CC3120MOD Other Parts Discussed in Thread: CC3120 , 4213 , UNIFLASH Tool/software: Code Composer Studio Hi all,
on an our device is mounted the CC3120MOD that is managed by an Tiva 32bit Microcontroller that work's on with Freertos and…
Hi Kaka,
Thank you for your patience. Please try using the following makefile:
4213.makefile.zip
This might produce an error in the console, but it should be silenced and not interfere with the library being built.
This issue will be resolved…
Hi Amir,
Sorry for the delayed response.
No I was not able to reproduce the issue of being able to scan public address advertisement but not private address advertisements in the 2.20 SDK. I think there is an issue somewhere else in your code. I have…
Patrick,
I received the replacement programming EVM and following the instructions:
6406.How to update to Win7 x64 Driver for Programming EVM.pdf
using the drivers here:
4213.Driver_ProgrammingEVM_Windows7.zip
I am now able to program the cdce706…
Hello Jared Casey.
Me too have similar query. Battery Terminal +(VBAT=3.7V) is connected to BAT pin of BQ27421 IC. We have used LDO for generating 3.3V to power the microcontoller and etc circuits.thew LDO input is VBAT where input to LDO is VBAT Voltage…