Part Number: ADS131M06 According to the datasheet. To write to a register you send: 011A AAAA ANNN NNNN
So I put on my TX buffer: 0x6180, to write to CLOCK which has an address of 0x03h (according to the datasheet) ie: 0110 0001 1000 0000
Making N…
Part Number: ADS131M06 Hi Ryan,
Sorry i was away for Long time and busy with other things.
Actually i am sensing AC Voltage of 540V with upper resistor of 900K and Bottom resistor of 2K.
so at ADC i am getting 1.2V when 540V is applied.
For continuous…
Part Number: ADS131M06 Hi,
Can you please help me in understanding noise level lost in conversions?
I wanted to measure 300VAC with the resolution of 1V
how i will make sure that with this ADC, I will achieve this resolution.
Regards,
Deepa…
Part Number: ADS131M06 Other Parts Discussed in Thread: ADS124S08 Hello Guys,
Good day.
Our customer is designing a board that requires 12 ADC channels, 6 are differential and 6 are single ended. Can the ADS131M06 be configured to support the 6 single…
Part Number: ADS131M06 Other Parts Discussed in Thread: ADS131A04 , ADS131A02 Can I use the ADS131M06 for 3-phase voltage /current signals with frequencies in the 10khz-30khz range?
Thanks
David Nyarko
Part Number: ADS131M06 Hi,
I am using ADS131M06 in one of my projects. If fault conditions occur I want to protect the ADC inputs from overvoltages. So to clamp overvoltages I want to follow a common approach of using Schottky diodes as shown in the…
Part Number: ADS131M06 Other Parts Discussed in Thread: ADS131M08 Hi Team,
There seems to be errors in the datasheet of the new devices, ADS131M06 and ADS131M08, regarding the maximum reference input voltage (REFIN). According to Section 6.1 Absolute…
Part Number: ADS131M06 Other Parts Discussed in Thread: SN6501 , ADS124S06 , ADS124S08 , ADS131M08 , LMT70 Hi,
I am looking for a simple ADC to be able to acquire several K thermocouples. Overall, the finished device should be able to evaluate 60…
Hi Aswin,
Please see below my comments regarding the two options you have listed out.
Please note that the VISO outputs of ISOW devices cannot be tied together directly. This is true for any DC power supply output, they can't be connected together…
Part Number: ADS131M04 Other Parts Discussed in Thread: AMC131M03 , , ADS131M06 Tool/software: Dear TI expert,
1. We are using ADS131M04 and facing issue with the received data. Many a times, received CRC is not correct in the received frame. Same…