Part Number: ADS1610 Hello HSADC team,
I have 2 questions about Group Delay of ADS1610.
Now customer is using ADS1610 but they facing a problem that ADS1610 seems to have around 20us group delay.
1. As I can see in datasheet page.4, typical value of group…
Other Parts Discussed in Thread: ADS1610 It seems ADS1610 is in NRND phase.
Our customer have been using this devices at following condition.
Could you please advice alternative?
OSR=3 / Output rate = 20MHz.
Because INL is key parameter, the pipe-lined…
Other Parts Discussed in Thread: ADS1610 How can i get the footprint symbol of ADS1610?
I tried Ultra Librarian 6.1.1 with 'ADS1610_PAP_64.bxl'.
but it doesn't work.
PADSTACK WARNINGS:
Drill hole size is equal or larger than smallest pad…
Other Parts Discussed in Thread: ADS1610 , DAC8820 , ADS1605 , AMC1200 Hi All,
We are planning to use an ADS1610 16-bit 10MSPS ADC converter in an application where it is connected back-to-back to a DAC8820, such that we can use a digital interface to galvanically…
Other Parts Discussed in Thread: ADS1610 Hello Everyone!
I had to make a 16-bit A/D converter that is acquiring data every 100ns for few seconds (over 10^7 samples). I decided to use ADS1610 but I am wondering how to store the data and further simply send…
Other Parts Discussed in Thread: ADS1610 If I need to vary the frequency of the ADS1610 clock for different same rates, what value of RBIAS should be used. The table in the data sheet specifies RBIAS values for fixed frequencies. Do I set the RBIAS for…
You are correct, but since these groups are always doing devices for the next rounds of test equipment they always have to do better than anything you can buy. In HD work, source cancellation methods are normally used, one of the very few published references…
Other Parts Discussed in Thread: ADS1610 Hi!
Can you tell me, why a high-speed precision ADC, like ADS1610, couldn't be used with an additional noise shaping, in order to create a nice audio ADC?
This converter's output features 16-bit with still almost…
Hi Tom,
I plan to interface ADS1610 (or ADS 1606 with FIFO disabled) to OMAP L138 via uPP using a breakout board .
I plan to connect the signals in the following way:
OMAP L138 uPP input ADS1610 Output
Clock <------------------------------------ DRDY…
Other Parts Discussed in Thread: AMC1305M25 , AMC1304M25 , ADS1118 , ADS1248 , TMS320F28377D , ADS5560 , ADS1610 , ADS5562 , AMC1210 HI,
I'm interested in the AMC1305M25 ADC chip, I'm hoping to achieve 16bit resolution at 20 MSps data conversion using this chip…