Part Number: AMC1304L05 Other Parts Discussed in Thread: TIDA-00080 , , AMC1304M25 Hi,
I have a customer that is looking at the TIDA-00080 design and wants to modify it by using a part that instead of shunt sensing (as the AMC1304) would just do voltage…
Part Number: AMC1304L05 Other Parts Discussed in Thread: AMC1210 , , SN65LVDS179 I´m in search of a single-chip simple as the AMC1210 to convert the bitreams out of AMC1304L05. the Problem is, that it seems to me that the AMC1210 only can communicate with…
Part Number: AMC1304L05 Hello,
according to the datasheet (revision 2017) the AMC1304L05 has a fail safe function. §8.4.1. Fail-Safe Output says: "In the case of a missing high-side supply voltage (LDOIN), ..." "Therefore, the AMC1304 implements…
Part Number: AMC1304L05 Hi,
I am currently testing a board using seven AMC1304L05 (for isolated current and voltage measurements) and have noticed a strange behaviour of the LVDS outputs. The ADCs are supplied with 5V on both sides.
No analog voltages…
Part Number: SN65LVDT14-EP Other Parts Discussed in Thread: AMC1304L05 , SN65LVDT14 Since the radiation problem, customer tried to create the bypass capacitor at the bias power rail from 0.1uF to 0.47uF. As a result, the radiation emission can be reduce…
Still having problems to aquire the data from the ADC. When measuring Data pin with the oscilloscope I get a sequence of ones and zeros, but when I approach the saturation Voltage (+50mV for the AMC1304L05), I still see a similar sequence of ones and…
Part Number: AMC1304L05 Hi,
does TI provide the FIT rate for the AMC1304L05DW?
As the device will be used in a SIL4 railway application the product's FIT rate has to be calculated. Although estimation might be sufficient if no exact value is avaliable…
Other Parts Discussed in Thread: AMC1304L05EVM , AMC1304L05 , AMC1200 Recently, I make some test with the demo board of AMC1304L05EVM , and use it in the half-bridge inverter circuit to measure output line current with the shunt.I have found that when the…
Other Parts Discussed in Thread: AMC1304L05 , ISO7842 Hello,
I am looking at the datasheet for the AMC1304L05 isolated delta-sigma modulator (document SBAS655C).
Figure 51 in the datasheet shows an application of the AMC1304 in a three phase inverter to…