Part Number: CD4046B Tool/software: I needed help regarding how do i generate sine wave from a square wave input to the PLL..... when i ordered i thout the VCO gives out a sine wave inherently but that is not the case ... so can you suggest a solution…
Part Number: CD4046B Hi,
Due to LM566 is obsolete, we want to check is there any possibility to replace LM566 with CD4046 VCO part.
The VCO part to be given with control voltage (12.37V at pin5), Resistor & Capacitor and receive output frequency of 155…
The inhibit pin disables the VCO, but the VCO output might stop in either the high or the low state. (I do not know what you're doing with the phase comparator; please show a schematic.)
As far as I can see, the CD4046B itself cannot put its output…
Part Number: CD4046B Dear All
We are a railway company and we use your PLL CD4046 in the acquisition of the speed of our trains.
An electronic board acquire impulses from speed sensors. There are 5 channels, as speed is acquired on 5 wheels.
The PLL deliver…
Part Number: CD4046B-MIL I would like to use this IC to demodulate FM signal at 240KHz
I am confusing with Datasheet.
Please let me know what will be the maximum and minimum for input as well as output voltage levels in rms?
Part Number: CD4046B We're looking for a 1ch and 2ch PLL, the speed can be from 100Mhz to 400Mhz with 3.3V bias power that is for FPGA. Could you help to find the appropriate one. very thanks.
Regards
Brian W
Part Number: CD4046B Other Parts Discussed in Thread: UCC21225A , , CD4518B , TCA6424A , SN74LV4046A Hi team
My customer wants to know whether TI has the solution to multiply a 100Hz input square wave signal to 100kHz (or at least 10kHz) output ?
The purpose…