Part Number: CDCE813-Q1 Other Parts Discussed in Thread: CDCE913 , , CDCE913-Q1 Hi Team,
I’m looking at the CDCE813 and CDCE913 do you have a document with the topline comparison table between these two parts/familes?
They appear to be the exact same…
Part Number: CDCE913-Q1 Other Parts Discussed in Thread: CDCE913 Hi Expert,
I have CDCE913 IC, configure through i2C.
I am able to get desired output frequency but my amplitude and pick to pick voltage is changing when i am changing the frequency. Is…
Part Number: CDCE913-Q1 Other Parts Discussed in Thread: CDCE913 Hi Sir/Madam,
Planning to use CDCE913-Q1 IC in our design. As per my understanding it accepts upto 1.9V clock input. My design need a part which accept 3.3V input clock signal.
Is it ok…
Part Number: CDCE913 Hi team,
Is it not necessary to connect to I2C when using this device in its default configuration? If not, please tell me about the pin handling.
Sincerely. Ryu
Part Number: TMDXIDK5718 Other Parts Discussed in Thread: CDCE913 , hello
I have a question about the TMDXIDK5718 evaluation board.
18pF is mounted on the load capacitors C172 and C173 of the crystal unit of U23 (CDCE913).
Is this 18pF because the register…
Part Number: CDCE913 Other Parts Discussed in Thread: CDCE6214 Hello TI experts,
My customer considers CDCE913 for their new product now.
the problem is, they use 3.3V input and output, and they only have 3.3V power rails,
But CDCE913 needs 1.8V for Vdd…
Part Number: CDCE913 Other Parts Discussed in Thread: CLOCKPRO hi ti team
How to config CDCE913 register to work with DS90UB941AS?
For example my video timing is 4096*781*60 and using 27M External Crystal.
Part Number: CDCE913-Q1 Other Parts Discussed in Thread: CDCE913 , CDCEL913-Q1 Hi team,
What is the difference between CDCE913-Q1 and non-Q1?
From the datasheet, I’ve found below listed is different:
Operational temperature
Thermal parameter
…
Part Number: CDCE913 Hello,
I am designing a system to generate MCLK for audio converters from external word clock (LRCLK). Your application note looks perfect for what I need but I need to support many word clock rates from 44.1k to 192k. I see in the…