Part Number: CDCE913-Q1 It is a question about the thermal pad of CDCEL913IPWRQ1. In the pin assignment diagram of datasheet P5, there is ThermalPad on the IC abdomen. However, there is no such pad in the part outline drawing of Datasheet P35 - 36. Is…
Part Number: CDCE913 Other Parts Discussed in Thread: CLOCKPRO Hello,Team, I have questions about CDCE913PW
Q1 Is there any latency between Y1 to Y2/Y3, when this devide is set to use Y1,Y2,Y3 from Pdiv1? or in that case,using Y1 with Pdiv1,Y2 with Pdiv2…
Part Number: CDCE913-Q1 Other Parts Discussed in Thread: CDCE925 , LMK03328 , CDCE6214 Hi,
19.2MHz is my input i need 4MHz, 25MHz and 12MHz clock outputs
does CDCE913-Q1 works for these parameters?
clock tree architect design tool not working.
Part Number: DS90UB941AS-Q1 Other Parts Discussed in Thread: CDCEL937-Q1 , CDCE913-Q1 , CDCE6214-Q1 , , DS90UH941AS-Q1 , CDCM6208 Hi,
If we use the External reference clock mode of DS90UB941AS, what's the recommended IC to provide the clear reference clock…
Part Number: DS90UB941AS-Q1 Other Parts Discussed in Thread: CDCE913-Q1 Hi Expert,
Our customer use 941 +948 in their project. Previously 941 uses DSI clock as input clock and it displays well. Then they use external clock as REFCLK which is generated…
Other Parts Discussed in Thread: CDCE913-Q1 Hi,
According to Datasheet of CDCE913-Q1, default setting of Sx(S0 to S2) is "0b001". This means that Y1_1 and FS1_1 will be used.
However, for PLL1, PLL1_0 will be used in default setting.
My customer…
Hello Zirui,
We recommend to select an adjustable clock generator with low jitter for this type of application such as CDCE913-Q1 or CDCE937-Q1. If both ports of the splitter use the same PCLK frequency then you could use a single PLL device such as CDCE913…
Part Number: CDCE813-Q1 Other Parts Discussed in Thread: CDCE913 , CLOCKPRO Hi team,
One of our customers uses the CDCE813 as a PCLK jitter cleaner with an input frequency of 24MHz.
I know it needs to operate in PLL mode if clock jitter cleaner is used.…
Part Number: CDCEL937-Q1 Other Parts Discussed in Thread: CDCE913 Hi experts,
Could you please help to share the IBIS model of CDCEL937-Q1? I only found the IBIS model of CDCE913 on ti.com, can they share the same IBIS model?
One more question, there…
Part Number: CDCS503-Q1 Other Parts Discussed in Thread: CDCE913-Q1 , CDCE6214-Q1 , CDCE913 , CDCE6214 , CDCEL913 Hi Sirs, Would you please provide a recommended part similar to CDCS503-Q1 but support 100MHz, 150MHz, 200MHz with +/-2% spread spectrum? Thank…