Part Number: CDCEL9XXPROGEVM Other Parts Discussed in Thread: CDCE913-Q1 , CLOCKPRO Hello Team,
Our customer trying to program CDCE913-Q1 by using CDCEL9XXPROGEVM board.
The D2,D3 LED is lighting so the LDO works correctly. But there seems no signal from…
Part Number: DS90UB941AS-Q1 Other Parts Discussed in Thread: CDCE913-Q1 Hi team,
For the single link 941AS, whether it can drive two different pixels screens with two different CLK ?
If it can be meet, how it should be implemented and what register configurations…
Part Number: CDCEL913-Q1 Other Parts Discussed in Thread: CDCE913-Q1 , CDCE6214-Q1 , CDCEL937-Q1 , CDCS503-Q1 Hi
The operational temperature range of CDCEL913-Q1 is only -40~85 while CDCE913-Q1 is -40~125, could you please tell me why? Any alternative part…
Part Number: CDCE813-Q1 Other Parts Discussed in Thread: CDCE913-Q1 , , CDCE913 Hi team,
If cdce813 could support 8.25MHz LVCMOS input, and output same 8.25MHz LVCMOS clock signal?
We want to clean the original PCLK jitter.
If it is possible, what do we…
Part Number: DLPC3435 Other Parts Discussed in Thread: CDCE913 Hi team,
I've got two questions regarding on DLPC3435 oscillator circuit. Could you please take a look below?
Q1: Which types of the oscillator (indicated by PLL_REFCLK_I,PLL_REFCLK_O) …
Hi Itoh,
PLL1707 is a very old part and is not recommended. CDCE813-Q1 is the same device with CDCE913-Q1 with different EEPROM (default configuration). You can use the EVM for CDCE913-Q1 instead. CDCE6214-Q1 is a newer part and is more recommended.
…
Hi Rock,
The newer devices are CDCE913, CDCE6214-Q1, LMK03318 and LMK05318. The four devices are listed in the order of overall jitter performance. LMK05318 has the best performance and CDCE913 has the worst. CDCE6214-Q1 is more recommended if its performance…
Part Number: LMK61A2-156M Other Parts Discussed in Thread: CDCE913 , CDCE6214 , CDCE6214-Q1 Hi team,
Do we have 75MHz OSC for output LVDS level with spread spectrum?
Roy
Other Parts Discussed in Thread: CDCE913 , CDCE6214-Q1 Hey Comm.,
I've got a nice project going on with generating programmable digital signals.
The problem that occured is that i want to increase the (Clock-)frequency of my signals.
Up till now it…
Part Number: CDCE913 Other Parts Discussed in Thread: CDCE6214-Q1 Hi All,
I'm not familiar with clock generator selection. Could you help select the suitable device to replace DSC557-04 or any user guide for selection tips?
Thanks.
Regards,
Roy
…