Other Parts Discussed in Thread: CDCLVC1106 Hi
I'd like to tell me the output current of CDCLVC1106.
Conditions for use:
VDD :3.3V
By frequency :22.2kHz,
coaxial cable (Or it's suitable.) using a clock is distributed to 6 of DUT
Best regards
Part Number: LMK1C1106 Other Parts Discussed in Thread: CDCLVC1106 Hi,
We intend to use LMK1C1106 to buffer a SPI clock that fans out at 50MHz to multiple ADCs. However, we are also thinking to use it for the MOSI signal, which is not a clock. Is this…
Other Parts Discussed in Thread: CDCLVC1106 Are there some which were specified as the maximum of the load capacitance (C_load) of CDCLVC1106?
There is an example of 2pF×n in a data sheet. Does it become a problem with a larger value? It will be…
Hi Ethan,
LMK1C1106 can be used for buffering SPI lines. Note, that you need up to 5 cycles (clock or data) to enable/disable the output.
Alternatively, you can look at CDCLVC1106 which has asynchronous en/disable.
regards,
Julian
Other Parts Discussed in Thread: CDCLVC1106 Hi,
I want to use a CDCLVC1106 to clock 4 Ethernet phys a Cyclone IV FPGA and a TI C28346 DSP on one board.
The clock frequency would be 25MHz. For the application (EtherCAT fieldbus) we need an oscillator w…
Yes, LMK00105 can support input clock frequencies down to DC (0 Hz) using a DC-coupled input interface. Even with 3.3V supply, they need use a voltage divider to attenuate 3.3V input to <2Vpp swing. Also, it is important for the input slew rate to…
Other Parts Discussed in Thread: CDCLVC1106 Hi Folks,
We are going to implement two ethernet ports (RMII) with AM335X. Our intention is to use only one 50MHz oscillator as source to four points: the REF_CLK of the two MACs on AM335X and the CLKIN input…
Bob,
I think you run a huge risk of slow rise/fall times, signal reflections, and reduced signal swing by driving 24 components from one clock driver output. The device inputs themselves amount to 24x4pf, but the actual split in the transmission line…
Part Number: CDCLVC1110 Hello support team,
I have a question regarding CDCLVC11xx.
- Can CDCLVC11xx drive a CMOS IC (Vcc = 3.3 V) whose input capacitance is 20 pF with 50 MHz clock signal?
The period of 50 MHz clock signal is 20 ns. So I think the minimum…