Hi Daveon,
I've received a TLV320ADC6140 from Proto Advantage on one of their adapters and I'm attempting to begin the series of experiment you requested today.
Right away I ran into a bit of a snag/issue that I don't quite understand. It had occurred…
Part Number: MCU-PLUS-SDK-AM243X We checked a new version of EtherNet/IP Adapter Demos in MCU-PLUS-SDK-AM243X Version 08.05.00.24.
I found that the Link Layer Discovery Protocol (LLDP) feature is not supported in EtherNet/IP Adapter Demos 2.01.00 .…
Hi Anant,
I am testing the device in breadboard using SOP8 to DIP8 adapter. I am using Analog Discovery 2 as a signal generator and oscilloscope. When I test with OPA2197 in the same setup, I get the same results as yours. However, I'm having…
Hi Christian,
We would like to mention another discovery. We have confirmed that the USB_P and USB_N pins are correctly connected to the GPIO4 and GPIO5 of the TPS25750 respectively. When we connected the BC1.2 adapter to our board, we did not see any…
Hi Mohamad,
What version of the bluetopia stm stack are you using? Did you follow the STM32 Discovery guide
/cfs-file/__key/communityserver-discussions-components-files/538/6505.Enable_5F00_STM32_5F00_Discovery.pdf
Kind Regards,
Rogelio
Benjamin
The connection detection or discovery is handled by the USB Type-C to HDMI Cable Adapter.
The Cable Adapter contains logic circuit to implement SOP communication of USB PD and support discovery.
The HDMI DDC and CEC using the USB Type…
Part Number: MCU-PLUS-SDK-AM243X We checked EtherNet/IP Adapter Demos in MCU-PLUS-SDK-AM243X Version 08.03.00.18.
I found that the Link Layer Discovery Protocol (LLDP) feature is not supported in EtherNet/IP Adapter Demos .
software-dl.ti.com/...…
Part Number: PROCESSOR-SDK-AM335X Hi,
I am building a sample environment for Ethernet/IP at "PRU-ICSS-EthernetIP_Adapter_01.00.03.04"
I found that the Link Layer Discovery Protocol (LLDP) feature is not supported in EtherNet/IP Adapter Demos.
In…
Thank you for your reply. I have a dedicated 18V power supply adapter for the MAX17853. The 3.3V from the LP powers the MAX17841. I am using the SPI decode function on the scope and save a history of the GUI commands. I have not made any discoveries yet…
Hi Michael,
Michael Krummsdorf said: Still I am unable to use the demo properly, because I can't get a DCP discovery response from it (software profinet master connected via ethernet to both pru2 phys, don't have pru1 routed to ethernet phys). I think…