Part Number: LMK01010 Other Parts Discussed in Thread: DS90LV019 , Hi Sirs,
Sorry to bother you.
We are survey LVDS divider.
Divider needs to be used with LVDS DS90LV019, only for CLK frequency division, could you help check LMK01010 is a suitable solution…
Part Number: DS90LV019 Other Parts Discussed in Thread: SN65LVDS179 Hello support team,
I need your help.
My customer is on evaluation for a combination of SN65LVDS179 and DS90LV019. However, they found sometimes DS90LV019 is broken as the LVDS input…
Part Number: DS90LV019 It is observed from the datasheet that the common mode voltage for the driver is 1V to 1.7V. Can anyone tell me the common mode voltage at receiver input for the device DS90LV019TMTC/NOPB? ?
DS90LV019TMTC/NOPB
Part Number: DS90LV019 One of our major products uses DS90LV019TMTC/NOPB and is showing issues in production. During testing, we are having 20% of our boards show noise with the part. Sometimes it is just on the two differential receive lines, and sometimes…
Other Parts Discussed in Thread: DS90LV019 Hello Team,
Can you provide the (IoH) and the (IoL) of the DS90LV019?
I did not see this in the datasheet.
Also, what is the Max Frequency of the DS90LV019? The datasheet says above 100Mbps however is there…
Other Parts Discussed in Thread: DS90LV019 Hello,
I want to use DS90LV019 as a transceiver between a LVDS device and ATXmega USART, which is a 3.3V device. I have enabled the Xmega Pull-Up resistor on RX pin, but still receiving unexpected data due to noise…
Other Parts Discussed in Thread: DS90LV019 Please let me know about max cable range of DS90LV019.
・Cable:CAT5
・Signaling rate:100Mbps
Best regards,
Satoshi
Other Parts Discussed in Thread: DS90LV019 , SN65LVDT2 , SN65LVDS2 As the title says. The DS90LV019 goes two-way so has extra space I won't be using, wondering if there are any smaller parts that do the same thing. Need this for multiple lines in a space…
Hi Juliette, Thank you for looking into this. I'm not sure about the software that they will be using. Is there a way to have the thermal resistances same as what have been done through this E2E thread?: https://e2e.ti.com/support/interface/f/interface…
Part Number: SN65LVDS049 Other Parts Discussed in Thread: SN65176B , DS90LV019 Hi TI team,
My customer want to use RS422 or RS485 communication with SN65LVDS049 between SN65176B.
Is there any compatibility problem?
Please check it.
Thanks!
Downey Kim.