Hello ? ?,
1. Please read the TRM Chapter 24.7 .
2. The USB port remains and SW creates an ethernet instance.
You can find more information about the internet gadget driver --> https://www.kernel.org/doc/html/v4.13/driver-api/usb/gadget.html
Now that…
Part Number: SW-EK-TM4C1294XL Tool/software: Code Composer Studio We would like to add ethernet LAN to our existing TM4C1294 boards, that currently use USB. However we would like to keep USB as well (don't need high-speed usb).
Examples from Tivaware…
Part Number: DP83822I Other Parts Discussed in Thread: AM3358 , Tool/software: Hi,
We use the DP83822I for the Ethernet transceiver in our AM3358 board, and now, we find our mass product have the below issue for some board:
1. The network cards can be correctly…
Hi,
Tony Tang said: #1. Why did not use TI DP83869 SGMII PHY on TDA4VH EVM? but used a none TI device VSC8514?
CPSW9G is exposed via ENET expansions connectors and there is on PHY on TI EVM for CPSW9G. VSC8514 is QSGMII PHY, it enables 4 Ports of CPSW9G…
Hi Hu,
Are you looking for linux driver? If so, linux driver for DP83867 could be found in the following link:
https://www.ti.com/tool/ETHERNET-SW
--
Regards,
Hillman Lin
Part Number: MCU-PLUS-SDK-AM243X Tool/software:
Hi Expert,
We are working on a PROFINET project using the MCU-PLUS-SDK-AM243X, version 08_03_00_18. The code works perfectly on the EVM board. On our custom board, we are using the KSZ9031RNX…
Hi Chaesok,
Q1:
I briefly looked over your schematic and it looks good, for a full schematic review please fill out the schematic checklist and return to me. It can be found under the Design Tools & Simulation Tab in the DP83826 Product Page.
https…
Hi,
CPSW Ethernet on the AM263P Control Card EVM depends on I2C2 to communicate with the IO Expander to set the select bits of a few MUXes to route the correct signals for CPSW Ethernet.
For CPSW Ethernet, the IO Expander sets the following signals:
…
Part Number: TDA4VM Tool/software: Hi:
We are working with a supplier who has developed it own ECU where the algorithm are implemented for image processing. We want to interface with their system transfering the images we have captured with our system…
Hi, Pedrhom,
Thank you very much for your reply.
I still have some questions,
1)Whether I can get the HW data stream (or raw adc data) first and then the SW data stream (point cloud data) during the frame cycle, as illustrated in the figure.
2)Can I…