Part Number: LOWPASSFILTER-CALC Other Parts Discussed in Thread: LM6154 The Filter design tool:
It is not possible to lock a amplifier.
It takes a lot of time to set it back each time.
Bug: It is not possible to lock E24 resitor and capicitors. When a…
Part Number: AFE8000 For simulation requirements needs we should have the internal RX and TX filters structure as detailed below:
The DUC interpolation filters coefficient for the two next scenarios:
375[MSPS] input signal that interpolating to 12…
Hi Hajo,
Hajo Krabbenhöft said: From what I understand, the TLV320ADC3101 uses a delta-sigma modulator with 128-times oversampling, which comes out at 6.144MHz raw sample clock for a final 48kHz digital signal.
This is correct. You can input a PWM signal…
Part Number: AFE7950EVM Hello Everyone,
I'd like to ask for help to achieve RX NCO switching via GPIO. I've already managed to change TX NCO this way, as written in this topic: https://e2e.ti.com/support/rf-microwave-group/rf-microwave/f/rf-microwave…
Hi Daniel,
I would suggest looking at section 8.3.8.3 of the AFE7950 datasheet. In this section you can see the different JESD modes supported by the AFE along with the difference input and output rates for the DACs and ADCs respectively. To get the max…
Part Number: AMC3330 Hi
I downloaded the TINA Spice sbam456b.
Filter 1 is what is on the EVM and what was default in the sbam456b circuit. R1=R2=10ohms C=10nf with a cutoff freq of 796kHz
Freq
Vin
Vout
Gain
Input Filter
Error = (Ideal - measured)…
Part Number: ULC1001-DRV290XEVM Other Parts Discussed in Thread: DRV2901 , ULC1001 Hi~
Customer is under evaluating ULC1001-DRV290XEVM board and got several question as below.,
1. At DRV2901,how to boost output voltage? When see bootstrap, looks charge…
Hello Steve,
Would you mind filling out the calculator spreadsheet with your requirements and also share your schematic?
LM25088-5088QUICK-CALC Calculation tool | TI.com
There could be a number of reasons for instability.
1, Loop compensation
2. No…
Hi Ram,
Ram said: If I increase the Over Sampling Ratio to 512 (now I have it at 128), reducing the data rate to 8 ksps, could I have a higher cut-off freq for Sinc3?
My answer: the cut-off frequency of Sinc filter can be calculated as f-3db = data rate…
Hi
Here is the update from the developer post SDK9.1 testing
We tried reproducing this bug.but unable to do on the latest ti-rt-linux-kernel Once both interfaces (eth1 and eth3) are synchronized using phc2sys. And PPS signal is generated. We see the LEDs…