Part Number: DRV10987 Other Parts Discussed in Thread: L293D , Hi Team,
Our customer is looking for a sample code for DRV10987. He is using DRV10987 together with STM32 but it doesn't respond to the I2C command as shown in the screenshot below. I have checked…
Part Number: MSP430G2553 Other Parts Discussed in Thread: L293D , Hello, I have started programming the MSP430G2553 recently. I am trying to make the dc motor rotate in either direction with a push of a button. The motor driver I am using is L293D. I got…
Iain,
First of all, I am sorry you are having issues with our device.
The DRV8873 has the diodes integrated...body diodes across the FETs. You can see this in multiple figures throughout the datasheet. The L293D (optional part number) also has the diodes…
Hello Luigi,
If you have a dual supply where each half has enough voltage to run the relay then a push/pull peripheral driver would work well. With a single supply an H driver is needed. H driver is more common. For low cost there is DRV8837. For easy…
Спасибо за ответ, DRV777 не подходит, та как нужно менять полярность сигнала управления реле.
Подскажите - нужно ли ставить дополнительные защитные диоды на выводы AOUT1, AOUT1 и BOUT1, BOUT12 ( DRV8835 ), как это реализовано в L293D, или достаточно внутренних…
Part Number: LAUNCHXL-F28379D Other Parts Discussed in Thread: L293D Tool/software: Code Composer Studio Hello,
I am using LAUNCHXL-F28379D for a motor applicaiton and I am using EPWM module to drive L293D (H-bridge) motor driver. The voltage magnitude…
Seema,
LM321 is not a good choice. I suggest these alternatives in order.
TLV1805, TLV1805-Q1 Comparators (not for high output current )
L293D Quadruple Half-H Drivers (needs a 5V supply, too)
DS3668 Quad Fault Protected Peripheral Driver (needs 5V…
Part Number: SN754410 Other Parts Discussed in Thread: DRV8844 , DRV8802 , , DRV8871 , DRV8870 , DRV8872 , L293 , DRV8876 , L293D , DRV8816 Hello,
I have a question regarding the quadruple half-H driver SN754410 . I have looked that this driver is old but it is active…
Part Number: MSP430FR2311 Other Parts Discussed in Thread: L293D , Hello I am going to say that I am very new to Embedded systems. I could have started with the arduino as everyone else seems to do but I wanted to really understand how MCUs work so I opted…
Part Number: MSP430F5529 Other Parts Discussed in Thread: L293D ,
Tool/software: Code Composer Studio
I have been trying to implement motor control using an L293D with an MSP430F5529. I am not able to rotate the motor for a specific time and make it stop…