Hi Carl ,
The slow rise time of the inputs signal you mentioned in your post , how slow is it ? It is not recommended to have slow transition rate input signal into the device for its inherent issues . I have attached an app note talking about it .…
I would assume that the new ZR parent would assign the network address based on Zigbee PRO 2012 Specification Section 3.6.1.6 (Distributed Address Assignment Mechanism):
A parent device that has a Cskip(d) value greater than 0 shall accept child devices…
Hi TER,
So far, we only have this document obtain from the local authority website and it doesn't mention about the 2 or 3 harmonic limits.
Class-Assignment-No-3-of-2015Latest.pdf
Possible that the IoT device need to meet the 915MHz band standard…
Hi Kang,
Apologize for the delay since we were3 on holiday yesterday.
I would check every control signal to see if one of these control signals is at the wrong level or the pull up or down that you think are there indeed they are installed. You can…
So I included the pp file And the command line is :
/opt/ti-rtos/am57xx/2.0/ti-cgt-c6000_8.1.3/bin/cl6x" -mv6600 -O3 --opt_for_speed=5 --include_path="/opt/ti-rtos/am57xx/2.0/ti-cgt-c6000_8.1.3/include" --include_path="/opt/ti-rtos/am57xx/2.0/mathlib_c66x_3_1_1_0…
The INA241 has high bandwidth and passes high-frequency noise. An output capacitor can reduce visible output noise. Large capacitors also attenuate fast current transients. Use an RC filter instead of only a capacitor. Try 100 ohm and 10 nF initially…
Allan
I want to provide a forewarning here that the support for JTAG devices is limited, as the original National Semiconductor group who supported this product no longer exists, thus limiting our in-depth knowledge about this device.
SCANSTA112 would…
this is the transceiver which i used
8816.SPI to CAN FD SBC + LIN.pdf
i checked the schematic of the transceiver pullup resistor (1kΩ) and a series diode to VSUP connected to LIN bus.
in the linSend() function i can checked the signal on oscilloscope…