Other Parts Discussed in Thread: LM96570 Hi,
I have some doubts in using the LM96570 IC.
1) In data sheet of LM96570 are mentioned as default values, so shall I assume those are the values of registers when powered up before programming through spi (4…
Hi Suresh,
1) The TX_SDK_V1 and TX_SDK_V2 are the only EVMs for TI's HV pulser.
2) TI internal has power module with power on/off sequence built in for the above mention EVMs. However, it's not for sale. We are trying to put the power module schematic…
Other Parts Discussed in Thread: LM96570 Hi can any one help me to write a program to LM96570 IC using C6678 EVM, i tried to implement using GPIO's
but i am not sure whether it is correct process or not,but some of the datasheets are suggesting to…
Other Parts Discussed in Thread: LM96570 Hi all,
In the LM96570 datasheet there is an information that the output propagation delay(Tod) is between 32 and 47.5ns (table on page 6).
Therefore, the [total delay]=[output propagation delay] + [programmed delay…
Other Parts Discussed in Thread: TMS320C6678 Hi,
I am writing programme in CCS for spi, I facing some problem in getting required output.
This is the my code:
**************************************************
#include <c6x.h> #include <stdint.h>…
Other Parts Discussed in Thread: TMS320C6678 Hi,
I need to programme the Beamformer and AFE and one more slave through the spi of c6678. Upto my knowledge among 80 i/o pins 65,63,67,69 pins refer to SPI. In The four pins only one is chip select pin.…
Other Parts Discussed in Thread: LM96570
I don't see any posts on this part here yet so I will be the first.
Page 6 of the data sheet shows read data as needing top be read on the rising edge of SCK. My scope waveforms show that I should be clocking…
Part Number: AFE5832 Other Parts Discussed in Thread: AFE5809 , LM96570 , , TX517 , TX810 I see that TI have a complete solution for 8 channel ultrasonic transducers using
AFE5809, LM96530, LM96550, LM96570.
But if I decide to use a solution for 32 channel…
Other Parts Discussed in Thread: LM96570 Sir/Madam
After I am giving the power supply of +1.8V to 1.8V pin in EVM board, I checked the voltage level in banana cable connector pin at TX-SDK-V2 EVM board. It showed +1.4V only but as per datasheet of LM96570…
Other Parts Discussed in Thread: LM96570 Sir/Madam,
After I am giving the power supply of +1.8V to 1.8V pin in EVM board, I checked the voltage level in banana cable connector cable pin at TX-SDK-V2 EVM board. It showed +1.4V only. but as per datasheet…