Other Parts Discussed in Thread: LMH1982 Is it possible to be request a copy of the source code for the micrcontroller on the evaluation board? I am trying to program a LMH1982 in my own application circuit but I cannot get it to reliably lock to my PAL…
Other Parts Discussed in Thread: LMH1982LMH1982 Application If the input format is 625i and the output format 1080i/50 ,then how to program the register and what is the programming sequence?
Other Parts Discussed in Thread: LMH1982 , LMH1983 Is it possible to program the LMH1982 to generate a 29.5MHz clock when genlocked to a PAL video signal, and to generate a 24.546MHz clock when genlocked to a NTSC signal?
These clock signals allow me…
Other Parts Discussed in Thread: LMH1983 , LMH1982 Both LMH1982 and LMH1983 have LVDS clock outputs.
These output clock may be DC coupled to differential inputs of FPGAs with 2.5V power rail. My concern is that if LVDS output may higher than 2.5V signal…
Part Number: LMH1983 Other Parts Discussed in Thread: LMH1982 , Hi
I want to use the part in GENLOCK mode .
My system provides H sync and V sync only to my circuit .
Can I ignore the Fin signal (as LMH1982) and use only the H V sync?
My inputs…
Other Parts Discussed in Thread: LMH1983 , LMH1982 Hi,
I am looking for alternative solution to ICS9173B IC from renesas
This is a genlock PLL IC, which I am using for my input HYNCH and output bit clock to be in sync
Please help if you have…
Part Number: LMH0340 Other Parts Discussed in Thread: LMH1982 , Hi,
We have received the IP requested but we didn't see any test bench for simulation.
We tried to provide some inputs but could get all the dependencies correct.
Can you please share…
Part Number: LMH1981 Other Parts Discussed in Thread: LMH1982 , I use the LMH1981 sync separator to pass HSOUT, VSOUT and FOUT to my FPGA. These signals are then fed through to the LMH1982. From time to time the LMH1982 loses reference, because there…
Part Number: LMH1982SQEEVAL Other Parts Discussed in Thread: LMH1982 Hi I bought a LMH1982 evaluation board. I connected it to a PC, but I can't get any detection message, at most I'm getting a "Not recognized USB device". I tried it with 3 computers…