Hi Vicente,
Thanks for your help.
It seems that LMK03318EVM is required to read the total current consumption from the TICS Pro S/W. However, the customer does not have the EVM.
Could you please provide the total current consumption for the customer's…
Hi Rodrigo,
The suggested clock generator EVM doesn’t meet our requirement as the output format it supports is only differential.
Can you suggest clock gnerator EVM based on below requirements as I have mentioned before in same thread?
clock…
Hello,
The online tool is no longer available. Please use PLLATINUMSIM-SW instead. The LMK03318 has an internal loop filter that is controlled by registers except for the C2_LF capacitor. This capacitor is external and can be adjusted as needed. Recommendations…
The STAT0 and STAT1 outputs are controlled by several registers (R13-17, R19, R27, R28, R45, R56). Use the TICS Pro GUI to easily configure the register settings for LMK03318. The GUI also works with LMK03318EVM if you plan to test on the evaluation module…
Hello JH,
Yes, the LOL and LOS in R13 indicate the current status, status at the moment of reading.
INT_FLAG register R16 can be used to see if the device ever flags LOS or LOL. INT_FLAG register is used along with INT_FLAG_POL (R15), INTCTL (R17) and…
Part Number: LMK03318 Other Parts Discussed in Thread: , USB2ANY I am planning to use the LMK03318 on a two channel 160 MSPS ADC data capture board and I’d like to program the clock settings using the built-in LMK03318 EEPROM.
I used the TICS Pro…
Hi Ruihong,
Are you using the LMK03318EVM and CodeLoader software? Which EEPROM page are you writing to?
Thank you for running the simple test to program the SRAM and EEPROM. After successfully programming the EEPROM, R136 increases by 1 and R137.5 will…
The EEPROM Pages are numbered Page 0 through Page 5. You select the EEPROM Page with pins GPIO2 and GPIO3; see page 13 of the LMK03318EVM User's Guide for the Page Select settings.
Kind regards, Lane
Other Parts Discussed in Thread: LMK03318 , LMK03318EVM , TICSPRO-SW I need an ADC clock at multiple of 85M; 340, 425 and 510MHz, jitter < 120femto-secs over 1k to 10MHz.. Whichever of the 3 freq selected, I want a fixed 85M - Div by 4,5 or 6. I have a 80M…
Hello Puneet,
I have an LMK03318EVM and I have the same problem.
The suggested work around (uninstall/install) doesn't work on my computer (Windows 7 64bit). And the LMK033 1 8EVM isn't supported by the TICSpro software.
Thanks in advance,
Ber…