Hi,
We are not oscillator expert, so cannot suggest much.
Other customers asked similar question in this thread before -
https://e2e.ti.com/support/data-converters-group/data-converters/f/data-converters-forum/1188502/ads1293-crystal-or-external-oscillator…
Hello Ali,
We currently do not have any automotive rated oscillators.
We do have a new LMK6C BAW oscillator that is similar to the SiT8924.
Here is the link to the product folder: LMK6C product folder
The LMK6C is pin to pin compatible with the SiT8924…
Hi Zach,
i agree with Parker, that the LMK6C might be too high performance. You can likely use an XO like the LMK6C to drive the XTAL1 pin instead of a Xtal.
But an Xtal is probably the best solution here.
regards,
Julian
Hi Angela,
We have a BAW oscillator which is LMK6C which is LVCMOS type with a 25 ppm frequency stability, it is not available in QFN package but instead in the following packages.
You can use an oscillator with 25 ppm frequency stability.
Regards,
V…
Part Number: LMK62E0-156M Other Parts Discussed in Thread: LMK6C , LMK6P Hi Team,
My customer needs a 156.25MHz clock for the DSP.
Besides LMK62E0-156M, is there any other recommendation? Better supply is required. Thanks.
Regards, Charlie
Hi,
The crystal oscillator used in EVM is ECS-41-18-5PXEN-TR
We don't have particular/alternative crystal suggestion.
One thing you could do is to contact and/or open a ticket at TI's Clocks&Timing->Oscillators department Clocks and Timers …
Part Number: LMK04031 Other Parts Discussed in Thread: LMK5B12204 , LMK04821 , LMK04832 , LMK6C , LMK6P , LMK00804B Hi Experts, Good day.
Our customer needs to generate 1x, 2x, and 4x multiples of Audio frequencies 45.1584MHz & 49.152MHz on a single output, multiple…
Part Number: LMK03328 Other Parts Discussed in Thread: CDCE6214 , CDCDB800 , CDCDB400 , LMK6C Dear Team,
May you give some substitute solution for me to replace IDT?
9FGP204BKLFT<-> LMK03328
Thanks a lot.
Jimmy
Hi Viktor,
The LMK60E2 has a typical stability of around 15 ppm when operating at room temperature and without aging effects. If you need a device with improved ppm tolerances, the LMK6C offers typical 10 ppm across all factors and 10 years of aging. There…